2022-03-07 07:46 AM
I struggle to use PDM Filter library.
This is the message error I get :
What I have done so far are : - in project properties, C/C++ general, Paths and syombols, in "Includes" I added the path to pdm2pcm_glo.h ; in "Library Paths" I added the path to a folder with all the libPDM_FIlter_CM3_GCC_wc16.A ... files.- Wrote #include "pdm2pcm_glo.h" in the main.
It's still not working :\
In "Paths and Symbols", in libraries, I think I can add a library but I don't know which one to use (all the files were included in mems1 folder). I tried randomly picking but I had another error message;
I am new to cubeIDE so it's very possible Im doing a beginner mistake here
Solved! Go to Solution.
2024-05-16 08:59 AM
Thanks @ghrairim the problem has solved.