2023-03-06 3:22 AM
Solved! Go to Solution.
2023-03-07 2:58 AM
Hi @ABulu.2 ,
you might check the iis2mdc_reg.c driver on github for the LSB to milliGauss conversion formula. I'm reporting them here for simplicity:
// Magnetometer raw data conversion
float_t iis2mdc_from_lsb_to_mgauss(int16_t lsb)
{
return ((float_t)lsb) * 1.5f;
}
// Temperature sensor raw data conversion
float_t iis2mdc_from_lsb_to_celsius(int16_t lsb)
{
return (((float_t)lsb / 8.0f) + 25.0f);
}
-Eleon
2023-03-06 11:47 AM
Welcome, @ABulu.2, to the community!
You forgot to specify the partnumber of the sensor, but from the description I could see that you probably use the IIS2MDC?
Let's see if @Eleon BORLINI can help you.
Regards
/Peter
2023-03-06 11:39 PM
Thank you for your return @Peter BENSCH . Yes, we use IIS2MDC. @Eleon BORLINI
2023-03-07 2:58 AM
Hi @ABulu.2 ,
you might check the iis2mdc_reg.c driver on github for the LSB to milliGauss conversion formula. I'm reporting them here for simplicity:
// Magnetometer raw data conversion
float_t iis2mdc_from_lsb_to_mgauss(int16_t lsb)
{
return ((float_t)lsb) * 1.5f;
}
// Temperature sensor raw data conversion
float_t iis2mdc_from_lsb_to_celsius(int16_t lsb)
{
return (((float_t)lsb / 8.0f) + 25.0f);
}
-Eleon
2023-03-07 4:12 AM
Thank you, and can we use below formula for calculate the amplitude value? Because these values are vector and we want to focused amplitude value.
2023-03-07 9:15 AM
Hi @ABulu.2 ,
yes for sure, to have the spatial intensity you can use that formula.
-Eleon
2023-03-07 11:10 PM
Thank you :) Other questions are, how we can sure the sensor calibration? We have 4 sensor and when we were testing, we measured different x, y, z value. And I want to ask, we measure some values, and this values unit is milligauss, but what we measure using magnetometer? I think magnetic flux strength, but I am not sure. @Eleon BORLINI @Peter BENSCH
2023-03-10 5:40 AM
Hi @ABulu.2 ,
regarding the different measure issue, our suggestion is to always run the hard iron compensation, that calibrates the sensor residual offset at Time 0. You can refer to this example for LIS2MDL --> lis2mdl_hard_iron.c, which is very similar to IIS2MDC at programming level.
Regarding the physical quantity measured, you are right, it is the magnetic induction or magnetic flux density.
-Eleon
2023-07-25 10:48 PM
Thanks for your support @Eleon BORLINI. My thesis topic is to develop a dynamic preventive maintenance schedule for medical devices based on their usage. For this purpose, I have been collecting data using a magnetometer sensor 24/7 for the past 3 months. I need guidance on how to analyze the data from the three axes. Standard deviation seems to provide accurate results in determining the duration of device usage. However, I am concerned about the presence of noise in the real data and the potential reasons for fluctuations. Could you provide insights on how to interpret the data and what percentage of error can be considered normal?
2023-07-25 10:49 PM
Thank you for your support @peter BENS. My thesis topic is to develop a dynamic preventive maintenance schedule for medical devices based on their usage. For this purpose, I have been collecting data using a magnetometer sensor 24/7 for the past 3 months. I need guidance on how to analyze the data from the three axes. Standard deviation seems to provide accurate results in determining the duration of device usage. However, I am concerned about the presence of noise in the real data and the potential reasons for fluctuations. Could you provide insights on how to interpret the data and what percentage of error can be considered normal?