cancel
Showing results for 
Search instead for 
Did you mean: 

Hi, This is a question regarding ISM330DLC What was the input given to the accelerometer (eg: 1g,2g,3g) and Gyroscope(eg: 0.1dps,1dps..) while measuring Linear acceleration sensitivity change vs. temperature & Angular rate sensitivity change vs. temp?

KJose.1
Associate II
 
1 ACCEPTED SOLUTION

Accepted Solutions
Eleon BORLINI
ST Employee

Hi @KJ.2ose​ ,

the input stimulus (1g in the case of the accelerometer, 100dps in the Gyroscope case) is provided to the devices during the temperature ramp.

Note that, as reported in the datasheet:

measurements are performed in a uniform temperature setup and they are based on characterization data in a limited number of samples. Not measured during final test for production.

-Eleon

View solution in original post

2 REPLIES 2
Eleon BORLINI
ST Employee

Hi @KJ.2ose​ ,

the input stimulus (1g in the case of the accelerometer, 100dps in the Gyroscope case) is provided to the devices during the temperature ramp.

Note that, as reported in the datasheet:

measurements are performed in a uniform temperature setup and they are based on characterization data in a limited number of samples. Not measured during final test for production.

-Eleon

Thank you Eleon