‎2023-04-24 12:36 PM
Solved! Go to Solution.
‎2023-04-25 11:03 AM
The marking of the ASM330LHHXTR is LC.
The groups of digits 213 or 307 stand for the date code in the form YWW, i.e. the last digit of the production year and two digits for the calendar week.
A digit can only be used to represent the year within a decade, but the ASM330LHHX was only launched in 2022, so 307, for example, represents calendar week 7 in 2023.
Hope that helps?
Regards
/Peter
‎2023-04-24 1:06 PM
@Billy OWEN​ please flag to appropriate parties
Documentation Fail, Marking Codes are a repetitive question
‎2023-04-25 10:52 AM
‎2023-04-25 11:03 AM
The marking of the ASM330LHHXTR is LC.
The groups of digits 213 or 307 stand for the date code in the form YWW, i.e. the last digit of the production year and two digits for the calendar week.
A digit can only be used to represent the year within a decade, but the ASM330LHHX was only launched in 2022, so 307, for example, represents calendar week 7 in 2023.
Hope that helps?
Regards
/Peter
‎2023-04-25 11:11 AM
‎2023-04-25 11:12 AM
Great, you're welcome!
If the problem is solved, please mark this thread as answered by selecting Select as best, as also explained here. This will help other users find that answer faster.
Good luck!
/Peter
‎2023-04-25 6:38 PM
Hi Peter
As your mention, PN: ASM330LHHXTR was only lauched in 2022, while our buyer is buying the part with DC 307 (Year 2023, week 07). Could you double check with the production history of this part to ensure we are buying correct part? I'm worry about the Counterfreit in the market.
Best regards
‎2023-04-26 2:14 AM
"was only lauched in 2022" here means that there was no ASM330LHHXTR before 2022, but only after. And 2023 is after that. ;)