2023-01-02 4:14 AM
Solved! Go to Solution.
2023-01-04 6:39 AM
Hi @Zenk91 ,
For a general explanation of the Qvar principle, you can refer to the AN5755 application note.
For a more specific explanation on the Qvar sensing embedded in the ILPS22QS, you can refer to the AN5764 application note, from p.35.
Hope this can help.
-Eleon
2023-01-04 6:39 AM
Hi @Zenk91 ,
For a general explanation of the Qvar principle, you can refer to the AN5755 application note.
For a more specific explanation on the Qvar sensing embedded in the ILPS22QS, you can refer to the AN5764 application note, from p.35.
Hope this can help.
-Eleon
2023-01-04 10:40 AM
Hi Eleon Borlini,
Thank you very much for your answer, I will read these application notes. Could you clarify me the following doubt, please? Fundamentally the Qvar functionality makes a voltage detection induced by the presence of the electrostatic field? Thank you very much.
Regards.
2023-01-05 3:27 AM
Good morning,
I opened the second link (AN5764) but it shows always AN5755 application note, maybe that's an error? Thank you.
2023-01-05 6:49 AM
Hi @Zenk91 ,
This is the correct link for AN5764, you can find it online:
>> Fundamentally the Qvar functionality makes a voltage detection induced by the presence of the electrostatic field?
That's correct, it can detect a contact or no-contact voltage.
-Eleon
2023-01-05 7:27 AM
Hi,
Thank you very much, your help was very precious!
Regards,
Fabio.