2025-04-27 8:04 PM - last edited on 2025-04-27 11:53 PM by Federica Bossi
Hello,
I am using a VL53L0X sensor with a NUCLEO-64 F411 board, and I am trying to achieve accurate measurements and low power consumption for the development of a LiDAR system.
I have one problem and one question:
Problem:
The measurements are a bit inaccurate. For example, when I measure an object at a real distance of 5 cm, the sensor detects it at around 7 cm. Also, for some objects beyond 20–25 cm, the readings become irregular.
Question:
I would like to use the sensor with interrupts, but the User Manual for the API is not very clear on how to implement the interrupt feature.
I am attaching my main.c file and the library I am using, which includes the API and its .h file.
Thank you very much for your help!
//This is the main.c
/* USER CODE BEGIN Header */
/**
******************************************************************************
* @file : main.c
* @brief : Main program body
******************************************************************************
* @attention
*
* Copyright (c) 2025 STMicroelectronics.
* All rights reserved.
*
* This software is licensed under terms that can be found in the LICENSE file
* in the root directory of this software component.
* If no LICENSE file comes with this software, it is provided AS-IS.
*
******************************************************************************
*/
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "main.h"
/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */
#include "uart.h"
#include "lidarvl53.h"
/* USER CODE END Includes */
/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */
/* USER CODE END PTD */
/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */
uint16_t milimetros;
float distancia;
char texto[100];
/* USER CODE END PD */
/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */
/* USER CODE END PM */
/* Private variables ---------------------------------------------------------*/
I2C_HandleTypeDef hi2c1;
UART_HandleTypeDef huart2;
/* USER CODE BEGIN PV */
/* USER CODE END PV */
/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_I2C1_Init(void);
static void MX_USART2_UART_Init(void);
/* USER CODE BEGIN PFP */
/* USER CODE END PFP */
/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */
/* USER CODE END 0 */
/**
* @brief The application entry point.
* @retval int
*/
int main(void) {
/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_I2C1_Init();
MX_USART2_UART_Init();
/* USER CODE BEGIN 2 */
lidar_init(dir_s1);
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1) {
distancia = lidar_lee_mm(dir_s1);
if (distancia < 0) {
uartx_write_text(&huart2, "SENSOR NO CONECTADO\n");
} else {
sprintf(texto, "\r%f cm\n", distancia); // 2 decimales
uartx_write_text(&huart2, texto);
}
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
}
/* USER CODE END 3 */
}
/**
* @brief System Clock Configuration
* @retval None
*/
void SystemClock_Config(void) {
RCC_OscInitTypeDef RCC_OscInitStruct = { 0 };
RCC_ClkInitTypeDef RCC_ClkInitStruct = { 0 };
/** Configure the main internal regulator output voltage
*/
__HAL_RCC_PWR_CLK_ENABLE();
__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);
/** Initializes the RCC Oscillators according to the specified parameters
* in the RCC_OscInitTypeDef structure.
*/
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
RCC_OscInitStruct.HSIState = RCC_HSI_ON;
RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_NONE;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK) {
Error_Handler();
}
/** Initializes the CPU, AHB and APB buses clocks
*/
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK | RCC_CLOCKTYPE_SYSCLK
| RCC_CLOCKTYPE_PCLK1 | RCC_CLOCKTYPE_PCLK2;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_HSI;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_0) != HAL_OK) {
Error_Handler();
}
}
/**
* @brief I2C1 Initialization Function
* None
* @retval None
*/
static void MX_I2C1_Init(void) {
/* USER CODE BEGIN I2C1_Init 0 */
/* USER CODE END I2C1_Init 0 */
/* USER CODE BEGIN I2C1_Init 1 */
/* USER CODE END I2C1_Init 1 */
hi2c1.Instance = I2C1;
hi2c1.Init.ClockSpeed = 400000;
hi2c1.Init.DutyCycle = I2C_DUTYCYCLE_2;
hi2c1.Init.OwnAddress1 = 0;
hi2c1.Init.AddressingMode = I2C_ADDRESSINGMODE_7BIT;
hi2c1.Init.DualAddressMode = I2C_DUALADDRESS_DISABLE;
hi2c1.Init.OwnAddress2 = 0;
hi2c1.Init.GeneralCallMode = I2C_GENERALCALL_DISABLE;
hi2c1.Init.NoStretchMode = I2C_NOSTRETCH_DISABLE;
if (HAL_I2C_Init(&hi2c1) != HAL_OK) {
Error_Handler();
}
/* USER CODE BEGIN I2C1_Init 2 */
/* USER CODE END I2C1_Init 2 */
}
/**
* @brief USART2 Initialization Function
* None
* @retval None
*/
static void MX_USART2_UART_Init(void) {
/* USER CODE BEGIN USART2_Init 0 */
/* USER CODE END USART2_Init 0 */
/* USER CODE BEGIN USART2_Init 1 */
/* USER CODE END USART2_Init 1 */
huart2.Instance = USART2;
huart2.Init.BaudRate = 115200;
huart2.Init.WordLength = UART_WORDLENGTH_8B;
huart2.Init.StopBits = UART_STOPBITS_1;
huart2.Init.Parity = UART_PARITY_NONE;
huart2.Init.Mode = UART_MODE_TX_RX;
huart2.Init.HwFlowCtl = UART_HWCONTROL_NONE;
huart2.Init.OverSampling = UART_OVERSAMPLING_16;
if (HAL_UART_Init(&huart2) != HAL_OK) {
Error_Handler();
}
/* USER CODE BEGIN USART2_Init 2 */
/* USER CODE END USART2_Init 2 */
}
/**
* @brief GPIO Initialization Function
* None
* @retval None
*/
static void MX_GPIO_Init(void) {
GPIO_InitTypeDef GPIO_InitStruct = { 0 };
/* USER CODE BEGIN MX_GPIO_Init_1 */
/* USER CODE END MX_GPIO_Init_1 */
/* GPIO Ports Clock Enable */
__HAL_RCC_GPIOA_CLK_ENABLE();
__HAL_RCC_GPIOB_CLK_ENABLE();
/*Configure GPIO pin : PA5 */
GPIO_InitStruct.Pin = GPIO_PIN_5;
GPIO_InitStruct.Mode = GPIO_MODE_IT_RISING;
GPIO_InitStruct.Pull = GPIO_NOPULL;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
/* EXTI interrupt init*/
HAL_NVIC_SetPriority(EXTI9_5_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(EXTI9_5_IRQn);
/* USER CODE BEGIN MX_GPIO_Init_2 */
/* USER CODE END MX_GPIO_Init_2 */
}
/* USER CODE BEGIN 4 */
/* USER CODE END 4 */
/**
* @brief This function is executed in case of error occurrence.
* @retval None
*/
void Error_Handler(void) {
/* USER CODE BEGIN Error_Handler_Debug */
/* User can add his own implementation to report the HAL error return state */
__disable_irq();
while (1) {
}
/* USER CODE END Error_Handler_Debug */
}
#ifdef USE_FULL_ASSERT
/**
* @brief Reports the name of the source file and the source line number
* where the assert_param error has occurred.
* file: pointer to the source file name
* line: assert_param error line source number
* @retval None
*/
void assert_failed(uint8_t *file, uint32_t line)
{
/* USER CODE BEGIN 6 */
/* User can add his own implementation to report the file name and line number,
ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
/* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */
//Archive .h
/*
* lidarvl53.h
*
* Created on: Jul 20, 2023
* Author: alcid
*/
#define lidar_max_mm 2000
#ifndef LIBERRIAS_VL53L0X_LIDARVL53_H_
#define LIBERRIAS_VL53L0X_LIDARVL53_H_
#define dir_s1 0x52 //direccion del 1° sensor
#define dir_s2 0x53 //direccion del 2° sensor
#define dir_s3 0x54 //direccion del 3° sensor
#define dir_s4 0x55 //direccion del 4° sensor
#define dir_s5 0x56 //direccion del 5° sensor
#define dir_s6 0x57 //direccion del 6° sensor
#define dir_s7 0x58 //direccion del 7° sensor
#define dir_s8 0x59 //direccion del 8° sensor
#include "vl53l0x_api.h"
#include "main.h"
void lidar_init(uint8_t dir);
float lidar_lee_mm(uint8_t dir);
float lidar_lee_cm(uint8_t dir);
uint8_t lidar_set_dir(uint8_t dir);
#endif /* LIBERRIAS_VL53L0X_LIDARVL53_H_ */
//Library
#include "lidarvl53.h"
#define HIGH_ACCURACY_MODE 200000
VL53L0X_RangingMeasurementData_t RangingData;
VL53L0X_Dev_t vl53l0x_c; // center module
VL53L0X_DEV Dev = &vl53l0x_c;
uint32_t refSpadCount;
uint8_t isApertureSpads;
uint8_t VhvSettings;
uint8_t PhaseCal;
extern I2C_HandleTypeDef hi2c1;
void lidar_init(uint8_t dir)
{
VL53L0X_Error Status = VL53L0X_ERROR_NONE;
Dev->I2cHandle = &hi2c1;//el puerto i2c a usar
Dev->I2cDevAddr = dir;
Dev->comms_type=1;
Dev->comms_speed_khz=400;// i2c a 400khz
VL53L0X_WaitDeviceBooted( Dev );
VL53L0X_DataInit( Dev );
VL53L0X_StaticInit( Dev );
VL53L0X_PerformRefSpadManagement(Dev, &refSpadCount, &isApertureSpads);
VL53L0X_PerformRefCalibration(Dev, &VhvSettings, &PhaseCal);
VL53L0X_SetDeviceMode(Dev, VL53L0X_DEVICEMODE_CONTINUOUS_RANGING);
// Enable/Disable Sigma and Signal check
if (Status == VL53L0X_ERROR_NONE) {
Status = VL53L0X_SetLimitCheckValue(Dev, VL53L0X_CHECKENABLE_SIGNAL_RATE_FINAL_RANGE,(FixPoint1616_t)(0.25*65536));
}
if (Status == VL53L0X_ERROR_NONE) {
Status = VL53L0X_SetLimitCheckValue(Dev,VL53L0X_CHECKENABLE_SIGMA_FINAL_RANGE,(FixPoint1616_t)(18*65536));
}
if (Status == VL53L0X_ERROR_NONE) {
Status = VL53L0X_SetMeasurementTimingBudgetMicroSeconds(Dev ,200000);
}
if(Status == VL53L0X_ERROR_NONE){
Status = VL53L0X_SetGpioConfig(Dev, 0, VL53L0X_DEVICEMODE_CONTINUOUS_RANGING, VL53L0X_GPIOFUNCTIONALITY_NEW_MEASURE_READY, VL53L0X_INTERRUPTPOLARITY_LOW);
}
if (Status == VL53L0X_ERROR_NONE) {
Status = VL53L0X_StartMeasurement(Dev);
}
}
float lidar_lee_mm(uint8_t dir)
{
float lidarmil;
float offset = 24.848;
Dev->I2cDevAddr = dir;
VL53L0X_GetRangingMeasurementData(Dev, &RangingData);
lidarmil = (float)RangingData.RangeMilliMeter - offset;
if (lidarmil > lidar_max_mm) lidarmil = lidar_max_mm;
return lidarmil;
}
float lidar_lee_cm(uint8_t dir)
{
return((float)lidar_lee_mm(dir)/10.0);
}
uint8_t lidar_set_dir(uint8_t dir)
{
uint8_t status = VL53L0X_SetDeviceAddress(Dev, dir << 1);
return(status);
}