cancel
Showing results for 
Search instead for 
Did you mean: 

Health monitoring wrist based device

ab.7
Associate II

Hi,

we are developing wrist based health monitoring device to measure following parameters.

1) Heart rate,Spo2,Blood pressure.

2) Gps Tracking.

3) Accelerometer.

Please suggest the sensor modules for measuring above parameters.

or suggest us if u have any product measuring above parameters.

1 REPLY 1
Eleon BORLINI
ST Employee

Hi @ab.7​ , I suggest you to read this article and check if the described product can be of your utility. It is a review-like article of an STM customer (so a third part article) on the use of the SensorTile.box tool as a wearable-oriented product. Unfortunately this does't allow the GPS tracking, because you would need at least wifi connection, so I would suggest you also this other tool, the STEVAL-STWINKT1, which is equipped from a wifi module. As regard the Sp02 devices, greatly requested in current worldwide situation, I believe that STMicroelectronics unfortunately doesn't offer a saturimeter in its portfolio. Regards