cancel
Showing results for 
Search instead for 
Did you mean: 

H3LIS331DL interrupt on threshold levels

David45
Associate II

Hi, 

 

I want to detect a shock  with the H3LIS331DL and its interrupt on threshold level. I used it in normal mode and an ODR of 1000Hz. The shock in my testbanch is : 

David45_0-1732636061082.png

I want to know what is the minimum of time when the duration is setup to 0 with my ODR to set interrupt signal.

What is the answer of the sensor when the shock is an high frequency one...

There is few information about the bandwidth of the sensor or about its transfer function in its datasheet or application note.

Thanks for your help

 

 

 

1 REPLY 1
Federica Bossi
ST Employee

Hi @David45 ,

You can't find information about bandwidth and transfer functions because they are confidential and require an NDA. To get them you could contact Online Support at this link.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.