2021-07-25 5:49 PM
Hi, what is the frequency range of IIS3DWB vibration sensor for velocity? Thanks!
Solved! Go to Solution.
2021-07-26 1:20 AM
For an harmonic motion (and for a generalized motion as well), the maximum frequency for the acceleration is the same as the velocity one.
https://en.wikipedia.org/wiki/Simple_harmonic_motion
For the IIS3DWB case, the maximum ODR is 26.67kHz, but the flat frequency response range is from DC to 6 kHz (±3 dB point) as stated in the datasheet, so 6kHz is also the maximum detectable frequency for the velocity.
https://www.st.com/resource/en/datasheet/iis3dwb.pdf
Tom
2021-07-26 1:20 AM
For an harmonic motion (and for a generalized motion as well), the maximum frequency for the acceleration is the same as the velocity one.
https://en.wikipedia.org/wiki/Simple_harmonic_motion
For the IIS3DWB case, the maximum ODR is 26.67kHz, but the flat frequency response range is from DC to 6 kHz (±3 dB point) as stated in the datasheet, so 6kHz is also the maximum detectable frequency for the velocity.
https://www.st.com/resource/en/datasheet/iis3dwb.pdf
Tom
2022-07-06 11:51 PM
Hello @Community member ,
ISM330DLC - 3D accelerometer, How to check the over limit vibrations?
Configured the sensor ISM330DLC - ODR set to max 6.6KHz (which is max limit for chip).
If sensor ISM330DLC is exposed for heavy vibrations in the range above 3.3kHZ, for example 4kHz.
Is there a way that sensor provides any information or register update to indicate to the user that vibration is over limited?
Please assist to solve the issue.
Regards,
Srinu