2021-05-05 9:17 AM
Hello everyone!
I got LSM6DSO on my custom board with stm32l4 MCU, I only use I2C interface (that i don't use interrupt). I'm using LSM6DSO free fall example code in STMems standard C drivers, I can get the id of LSM6DSO so i think the I2C interface is working fine, I have tried doing some free fall test (drop it from my hand) but the FF_IA in WAKE_UP_SRC kept staying 0) so the free fall can't be detected.
Can anyone help me?
Solved! Go to Solution.
2021-05-05 10:44 PM
Hi @DDuc .1 ,
did you configure the wake-up interrupt?
I ask this, because the register you are reading is for the wake-up
you should check the FF_IA bit in register ALL_INT_SRC (1Ah)
also can you confirm that you set the INTERRUPTS_ ENABLE bit in register TAP_CFG2 (58h)?
even if you do not route the interrupts on INT1 or INT2, you have to set it to let the free-fall trigger
I hope this helps
Niccolò
2021-05-05 10:44 PM
Hi @DDuc .1 ,
did you configure the wake-up interrupt?
I ask this, because the register you are reading is for the wake-up
you should check the FF_IA bit in register ALL_INT_SRC (1Ah)
also can you confirm that you set the INTERRUPTS_ ENABLE bit in register TAP_CFG2 (58h)?
even if you do not route the interrupts on INT1 or INT2, you have to set it to let the free-fall trigger
I hope this helps
Niccolò
2021-05-06 9:04 PM
Hi @niccolo.ruffini
Your configuring the wake-up interrupt suggestion really help me a lot, I have configured wake-up interrupt and it worked! The FF_IO in WAKE_UP_SRC turn to 1 as my expectation.
Beside, I have checked the FF_IO from ALL_INT_SRC instead of WAKE_UP_SRC bit it didn't go to 1 when I tested free-fall (even I routed the interrupt). Do you know why ?
Thanks for your big help!
2021-05-07 12:46 AM
Hi @DDuc .1 ,
you are welcome, I'm glad to hear it worked =)
regarding the ALL_INT_SRC it can depend on how you configured other registers.
depending on your configuration I figured one of the two suggestion was right.
if you want we can dig deep into it.
Niccolò
p.s. if the problem is solved, you can select a best answer to help other members of the community with similar problems
2021-05-07 1:49 AM
Hi @niccolo.ruffini
My configuration just exactly like lsm6dso free fall example, and I have uncomment generation interrupt from int1 pin just like this. It is great if you can dig deep into it to confirm the example is working fine, I will do some investigation on my code too (may be my implementation was wrong in someway).
/* Disable I3C interface */
lsm6dso_i3c_disable_set(&dev_ctx, LSM6DSO_I3C_DISABLE);
/* Set XL Output Data Rate */
lsm6dso_xl_data_rate_set(&dev_ctx, LSM6DSO_XL_ODR_417Hz);
/* Set 2g full XL scale */
lsm6dso_xl_full_scale_set(&dev_ctx, LSM6DSO_2g);
/* Enable LIR */
lsm6dso_int_notification_set(&dev_ctx, LSM6DSO_ALL_INT_LATCHED);
/* Set Free Fall duration to 3 and 6 samples event duration */
lsm6dso_ff_dur_set(&dev_ctx, 0x06);
lsm6dso_ff_threshold_set(&dev_ctx, LSM6DSO_FF_TSH_312mg);
lsm6dso_pin_int1_route_get(&dev_ctx, &int1_route);
int1_route.reg.md1_cfg.int1_ff = PROPERTY_ENABLE;
lsm6dso_pin_int1_route_set(&dev_ctx, &int1_route);Thanks again for your big help!
2021-05-07 8:20 AM
Hi @DDuc .1 ,
can you confirm the content of register MD1_CFG (5Eh)?
it should be set to 10h, but we can be sure with a read while the program is running =)
Niccolò
2021-11-12 3:36 AM
Hi, I am not getting the free fall in lis12dh12. please help me. not raised any interrupt?
Regards,
Ani
2021-11-15 5:24 AM
Hi Ani @Akuma.6 ,
did you follow all the steps like you did for lsm6dso?
Niccolò
2021-11-16 3:53 AM
Hi niccolo,
Thanks for your response. I have followed the below application note document for reading the interrupt. But lo luck.
dt0100-setting-up-freefall-recognition-with-sts-mems-accelerometers-stmicroelectronics.pdf
Regards,
Ani
2021-11-18 12:21 AM
Hi Ani @Akuma.6 ,
please, can you confirm that the registers are written correctly after the procedure?
Niccolò