cancel
Showing results for 
Search instead for 
Did you mean: 

For the MLC, how can the IMU work independently from the microcontroller and wake it up with an interrupt?

Evelina CAMILLERI
ST Employee

[webinar - Program decision trees in sensors with a Machine Learning Core]

1 REPLY 1
Evelina CAMILLERI
ST Employee

Once the MLC is configured to run on the device, the MLC keeps generating results (every MLC ODR) on the MLCx_SRC registers. The device generates an interrupt signal when a change of result occurs in one of these registers, in this way the microcontroller can be waken up to read the new result generated by the MLC.