cancel
Showing results for 
Search instead for 
Did you mean: 

For LIS3DH 3-axis accelerometer, what is the CS input pin's maximum input leakage current spec?

KWibl
Associate

I have a battery-based application, so I want to minimize power, by selecting the largest-valued pullup resistor on the CS pin, that will guarantee a high on the input.

I cannot calculate this without knowing the maximum input leakage current on the CS input pin, but I cannot find that spec in the datasheet.'

How would I find this number?

Kevin

1 REPLY 1
Aishwarya
Associate III

LIS2DTW12 I²C/SPI mode selection

I want to read LIS2DTW12 data using SPI which is also shared with another device, can I use the LIS2DTW12 CS pin as chip select and operate devices one by one.

because according to the LIS2DTW12 datasheet:

State of CS

1: SPI idle mode / I²C communication enabled;

0: SPI communication mode / I²C disabled

i.e if cs = 1 --> I2C Enabled, read/write operation on another device will disturb the LIS2DTW12 device.