2021-04-21 4:17 PM
Hello, according to the datasheet for the LPS22HH, in Table 3 the temperature sensor operating range is -40C to +85C. Further down, it specifies that the temperature sensor absolute accuracy is +/- 1.5C from 0C to 80C.
What is the accuracy from -40C to 0C?
Thanks,
Derek
Solved! Go to Solution.
2021-04-22 2:52 AM
Hi Derek @smithderek2000 ,
below 0°C the accuracy is a little worse, probabily because it is more difficult to test in a humidity controlled environment, but nevertheless it is inside +-2.5°C (data from bench measures on representative samples), and almost across all the declared pressure range.
If my reply answered your question, please click on Select as Best at the bottom of this post. This will help other users with the same issue to find the answer faster.
-Eleon
2021-04-22 2:52 AM
Hi Derek @smithderek2000 ,
below 0°C the accuracy is a little worse, probabily because it is more difficult to test in a humidity controlled environment, but nevertheless it is inside +-2.5°C (data from bench measures on representative samples), and almost across all the declared pressure range.
If my reply answered your question, please click on Select as Best at the bottom of this post. This will help other users with the same issue to find the answer faster.
-Eleon