cancel
Showing results for 
Search instead for 
Did you mean: 

Enable vibrometer in STWINKT1B

PD
Associate

Hello Everyone,
In STWINKT1B, I need to enable the IIS3ZDWB sensor (vibrometer) and should be able to measure vibration of the given object with my phone via Bluetooth but the ST BLE Sensor Classic app is only showing the environmental parameters.

Can anyone help me in this please?

1 REPLY 1
SimonePradolini
ST Employee

Hi @PD 

STWIN default firmware is not enabling the IIS3DWB sensor. You must update manually the firmware.

FP-SNS-DATALOG1 is the best solution to log data. You can control the board configuration via the same BLE Sensor Classic app and save data via USB to a PC or onto a proper SD card. Here you can find the package and here User Manual and Quick Start Guide, where you can find also how to flash and update the firmware.

Best regards

Simone

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.