2018-12-19 2:03 PM
Using CubeMX v5.0 and FW_L0_v1.11.0 I'm generating new project from scratch.
Project has initialized (using HAL) UART2, I2C1 (on alternate pins PB8, PB9), GPIOs, EXTIs and clock. UART2, I2C1 and EXTI interrupts are enabled and IRQ handlers generated by the CubeMX.
On top of that there is X-CUBE-MEMS1 v5.2.1 with IKS01A2 extension and Application IKS01A2-DataLogTerminal. Project is generated for board NUCLEO-L053R8.
Just generated project couldn't be build. There is an error inside stm32l0xx_it.c, in function `USART2_IRQHandler()` error: "Undefined reference to huart2".
Same problem if this project is built for MDK-ARM v5.
CubeMX project file is attached. It's easy to regenerate the project.
I've tried to manually add #include or something in a hope that huart2 would become visible, but this BSP+MEMS1 Application seems like overcomplicated non-modular intertwined firmware. It's too hard to understand.
Please, can someone help me about this, just to make first build.
2018-12-19 4:01 PM
If it is a single undefined in another source file surely just defining it as an extern would suffice, unless it is a static in main.c
2018-12-20 5:07 AM
This works, but now I have problem with the Hard Fault. I'm debugging without IKS01A2 connected.
FW executes until the point when in need to initialize MX_Cube_MEMS1:
MX_X_CUBE_MEMS1_Init(void) --> MX_IKS01A2_DataLogTerminal_Init() --> IKS01A2_MOTION_SENSOR_GetCapabilities(i, &MotionCapabilities[i]) -->
int32_t IKS01A2_MOTION_SENSOR_GetCapabilities(uint32_t Instance, IKS01A2_MOTION_SENSOR_Capabilities_t *Capabilities)
{
int32_t ret;
if (Instance >= IKS01A2_MOTION_INSTANCES_NBR)
{
ret = BSP_ERROR_WRONG_PARAM;
}
else if (MotionDrv[Instance]->GetCapabilities(MotionCompObj[Instance], Capabilities) != BSP_ERROR_NONE)
{
ret = BSP_ERROR_UNKNOWN_COMPONENT;
}
else
{
ret = BSP_ERROR_NONE;
}
return ret;
}
The line `else if (MotionDrv[Instance]->GetCapabilities(MotionCompObj[Instance], Capabilities) != BSP_ERROR_NONE)` produces Hard Fault exception.
I have X-NUCLEO-IKS01A1, so there is a task awaiting :) - to port IKS01A1 code to this project and see if Hard Fault will be produced then.
2018-12-21 6:55 AM
Dear Mario,
I suggest you to
and the go to folder
STMicroelectronics.X-CUBE-MEMS1.5.2.1\Projects\STM32L053R8-Nucleo\Examples\IKS01A2\DataLogTerminal
The DataLogTerminal.ioc should have the right settings to solve your problem.
@parata.carlo for any follow-up.
Best regards,
Luca
2018-12-21 7:03 AM
#MicroXplorer Configuration settings - do not modify
File.Version=6
I2C1.I2C_Speed_Mode=I2C_Fast
I2C1.IPParameters=I2C_Speed_Mode,Timing
I2C1.Timing=0x00000000
KeepUserPlacement=true
Mcu.Family=STM32L0
Mcu.IP0=I2C1
Mcu.IP1=NVIC
Mcu.IP2=RCC
Mcu.IP3=SYS
Mcu.IP4=USART2
Mcu.IPNb=5
Mcu.Name=STM32L053R(6-8)Tx
Mcu.Package=LQFP64
Mcu.Pin0=PC13
Mcu.Pin1=PC14-OSC32_IN
Mcu.Pin10=PB8
Mcu.Pin11=PB9
Mcu.Pin12=VP_SYS_VS_Systick
Mcu.Pin13=VP_STMicroelectronics.X-CUBE-MEMS1_VS_BoardOoExtensionJjMEMS_5.2.1
Mcu.Pin14=VP_STMicroelectronics.X-CUBE-MEMS1_VS_DeviceJjApplication_5.2.1
Mcu.Pin2=PC15-OSC32_OUT
Mcu.Pin3=PH0-OSC_IN
Mcu.Pin4=PH1-OSC_OUT
Mcu.Pin5=PA2
Mcu.Pin6=PA3
Mcu.Pin7=PA5
Mcu.Pin8=PA13
Mcu.Pin9=PA14
Mcu.PinsNb=15
Mcu.ThirdParty0=STMicroelectronics.X-CUBE-MEMS1.5.2.1
Mcu.ThirdPartyNb=1
Mcu.UserConstants=
Mcu.UserName=STM32L053R8Tx
MxCube.Version=5.0.0
MxDb.Version=DB.5.0.0
NVIC.EXTI4_15_IRQn=true\:0\:0\:false\:false\:true\:true
NVIC.HardFault_IRQn=true\:0\:0\:false\:false\:true\:false
NVIC.NonMaskableInt_IRQn=true\:0\:0\:false\:false\:true\:false
NVIC.PendSV_IRQn=true\:0\:0\:false\:false\:true\:false
NVIC.SVC_IRQn=true\:0\:0\:false\:false\:true\:false
NVIC.SysTick_IRQn=true\:0\:0\:true\:false\:true\:true
PA13.GPIOParameters=GPIO_Label
PA13.GPIO_Label=TMS
PA13.Locked=true
PA13.Mode=Serial_Wire
PA13.Signal=SYS_SWDIO
PA14.GPIOParameters=GPIO_Label
PA14.GPIO_Label=TCK
PA14.Locked=true
PA14.Mode=Serial_Wire
PA14.Signal=SYS_SWCLK
PA2.GPIOParameters=GPIO_Label
PA2.GPIO_Label=USART_TX
PA2.Locked=true
PA2.Mode=Asynchronous
PA2.Signal=USART2_TX
PA3.GPIOParameters=GPIO_Label
PA3.GPIO_Label=USART_RX
PA3.Locked=true
PA3.Mode=Asynchronous
PA3.Signal=USART2_RX
PA5.GPIOParameters=GPIO_Label
PA5.GPIO_Label=LD2 [Green Led]
PA5.Locked=true
PA5.Signal=GPIO_Output
PB8.Locked=true
PB8.Mode=I2C
PB8.Signal=I2C1_SCL
PB9.Locked=true
PB9.Mode=I2C
PB9.Signal=I2C1_SDA
PC13.GPIOParameters=GPIO_Label,GPIO_ModeDefaultEXTI
PC13.GPIO_Label=B1 [Blue PushButton]
PC13.GPIO_ModeDefaultEXTI=GPIO_MODE_IT_FALLING
PC13.Locked=true
PC13.Signal=GPXTI13
PC14-OSC32_IN.Locked=true
PC14-OSC32_IN.Mode=LSE-External-Oscillator
PC14-OSC32_IN.Signal=RCC_OSC32_IN
PC15-OSC32_OUT.Locked=true
PC15-OSC32_OUT.Mode=LSE-External-Oscillator
PC15-OSC32_OUT.Signal=RCC_OSC32_OUT
PCC.Checker=true
PCC.Line=STM32L0x3
PCC.MCU=STM32L053R(6-8)Tx
PCC.PartNumber=STM32L053R8Tx
PCC.Seq0=0
PCC.Series=STM32L0
PCC.Temperature=25
PCC.Vdd=null
PH0-OSC_IN.Locked=true
PH0-OSC_IN.Mode=HSE-External-Clock-Source
PH0-OSC_IN.Signal=RCC_OSC_IN
PH1-OSC_OUT.Locked=true
PH1-OSC_OUT.Signal=RCC_OSC_OUT
PinOutPanel.RotationAngle=0
ProjectManager.AskForMigrate=true
ProjectManager.BackupPrevious=false
ProjectManager.CompilerOptimize=6
ProjectManager.ComputerToolchain=false
ProjectManager.CoupleFile=false
ProjectManager.CustomerFirmwarePackage=
ProjectManager.DefaultFWLocation=true
ProjectManager.DeletePrevious=true
ProjectManager.DeviceId=STM32L053R8Tx
ProjectManager.FirmwarePackage=STM32Cube FW_L0 V1.11.0
ProjectManager.FreePins=false
ProjectManager.HalAssertFull=false
ProjectManager.HeapSize=0x200
ProjectManager.KeepUserCode=true
ProjectManager.LastFirmware=true
ProjectManager.LibraryCopy=0
ProjectManager.MainLocation=Src
ProjectManager.NoMain=false
ProjectManager.PreviousToolchain=
ProjectManager.ProjectBuild=false
ProjectManager.ProjectFileName=Test_Bug.ioc
ProjectManager.ProjectName=Test_Bug
ProjectManager.StackSize=0x400
ProjectManager.TargetToolchain=EWARM V8
ProjectManager.ToolChainLocation=
ProjectManager.UnderRoot=false
ProjectManager.functionlistsort=1-MX_GPIO_Init-GPIO-false-HAL-true,2-SystemClock_Config-RCC-false-HAL-false,3-MX_USART2_UART_Init-USART2-false-HAL-true,4-MX_I2C1_Init-I2C1-false-HAL-true,3-MX_X_CUBE_MEMS1_Init-STMicroelectronics.X-CUBE-MEMS1.5.2.1-false-HAL-true,4-MX_X_CUBE_MEMS1_Process-STMicroelectronics.X-CUBE-MEMS1.5.2.1-false-HAL-true
RCC.48CLKFreq_Value=24000000
RCC.AHBFreq_Value=2097000
RCC.APB1Freq_Value=2097000
RCC.APB1TimFreq_Value=2097000
RCC.APB2Freq_Value=2097000
RCC.APB2TimFreq_Value=2097000
RCC.FamilyName=M
RCC.HSE_VALUE=8000000
RCC.HSI16_VALUE=16000000
RCC.HSI48_VALUE=48000000
RCC.HSI_VALUE=16000000
RCC.I2C1Freq_Value=2097000
RCC.IPParameters=48CLKFreq_Value,AHBFreq_Value,APB1Freq_Value,APB1TimFreq_Value,APB2Freq_Value,APB2TimFreq_Value,FamilyName,HSE_VALUE,HSI16_VALUE,HSI48_VALUE,HSI_VALUE,I2C1Freq_Value,LCDFreq_Value,LPTIMFreq_Value,LPUARTFreq_Value,LSI_VALUE,MSI_VALUE,PLLCLKFreq_Value,PWRFreq_Value,RTCFreq_Value,RTCHSEDivFreq_Value,SYSCLKFreq_VALUE,TIMFreq_Value,USART1Freq_Value,USART2Freq_Value,VCOOutputFreq_Value,WatchDogFreq_Value
RCC.LCDFreq_Value=37000
RCC.LPTIMFreq_Value=2097000
RCC.LPUARTFreq_Value=2097000
RCC.LSI_VALUE=37000
RCC.MSI_VALUE=2097000
RCC.PLLCLKFreq_Value=24000000
RCC.PWRFreq_Value=2097000
RCC.RTCFreq_Value=37000
RCC.RTCHSEDivFreq_Value=4000000
RCC.SYSCLKFreq_VALUE=2097000
RCC.TIMFreq_Value=2097000
RCC.USART1Freq_Value=2097000
RCC.USART2Freq_Value=2097000
2018-12-21 7:03 AM
RCC.VCOOutputFreq_Value=48000000
RCC.WatchDogFreq_Value=37000
SH.GPXTI13.0=GPIO_EXTI13
SH.GPXTI13.ConfNb=1
STMicroelectronics.X-CUBE-MEMS1.5.2.1.ApplicationCcDeviceJjApplication=IKS01A2IiDataLogTerminal
STMicroelectronics.X-CUBE-MEMS1.5.2.1.BSP.number=4
STMicroelectronics.X-CUBE-MEMS1.5.2.1.BoardOoExtensionJjMEMS.apiComponent0=Board Extension\:IKS01A2
STMicroelectronics.X-CUBE-MEMS1.5.2.1.BoardOoExtensionJjMEMS.apiDoc0=Documentation/X_CUBE_MEMS1.chm
STMicroelectronics.X-CUBE-MEMS1.5.2.1.BoardOoExtensionJjMEMS.cmp_version0=5.2.1
STMicroelectronics.X-CUBE-MEMS1.5.2.1.BoardOoExtensionJjMEMS.component0=Board Extension
STMicroelectronics.X-CUBE-MEMS1.5.2.1.BoardOoExtensionJjMEMS.description0=MEMS library for X-NUCLEO-IKS01A2,X-NUCLEO-IKS01A2 BSP component drivers
STMicroelectronics.X-CUBE-MEMS1.5.2.1.BoardOoExtensionJjMEMS.diagnostic0=This component should operate correctly.
STMicroelectronics.X-CUBE-MEMS1.5.2.1.BoardOoExtensionJjMEMS.documentation0=Documentation/STMicroelectronics.X-CUBE-MEMS1_GettingStarted.pdf
STMicroelectronics.X-CUBE-MEMS1.5.2.1.BoardOoExtensionJjMEMS.group0=IKS01A2
STMicroelectronics.X-CUBE-MEMS1.5.2.1.BoardOoExtensionJjMEMS.paramName0=MEMSCcBoardOoExtensionJjIKS01A2
STMicroelectronics.X-CUBE-MEMS1.5.2.1.BoardOoExtensionJjMEMS.sevirity0=none
STMicroelectronics.X-CUBE-MEMS1.5.2.1.BoardOoExtensionJjMEMS_Checked=true
STMicroelectronics.X-CUBE-MEMS1.5.2.1.BoardOoExtensionJjMEMS_apiSize=1
STMicroelectronics.X-CUBE-MEMS1.5.2.1.BoardOoExtensionJjMEMS_bundle=MEMS
STMicroelectronics.X-CUBE-MEMS1.5.2.1.BoardOoExtensionJjMEMS_class=BoardOoExtension
STMicroelectronics.X-CUBE-MEMS1.5.2.1.BoardOoExtensionJjMEMS_name=X-CUBE-MEMS1
STMicroelectronics.X-CUBE-MEMS1.5.2.1.BoardOoExtensionJjMEMS_size=1
STMicroelectronics.X-CUBE-MEMS1.5.2.1.BoardOoExtensionJjMEMS_vendor=STMicroelectronics
STMicroelectronics.X-CUBE-MEMS1.5.2.1.BoardOoExtensionJjMEMS_version=5.2.1
STMicroelectronics.X-CUBE-MEMS1.5.2.1.DeviceJjApplication.apiComponent0=Board Extension\:IKS01A2
STMicroelectronics.X-CUBE-MEMS1.5.2.1.DeviceJjApplication.apiDoc0=Documentation/X_CUBE_MEMS1.chm
STMicroelectronics.X-CUBE-MEMS1.5.2.1.DeviceJjApplication.cmp_version0=5.2.1
STMicroelectronics.X-CUBE-MEMS1.5.2.1.DeviceJjApplication.component0=Device
STMicroelectronics.X-CUBE-MEMS1.5.2.1.DeviceJjApplication.description0=MEMS library applications,DataLogTerminal sample application for X-NUCLEO-IKS01A2
STMicroelectronics.X-CUBE-MEMS1.5.2.1.DeviceJjApplication.diagnostic0=This component should operate correctly.
STMicroelectronics.X-CUBE-MEMS1.5.2.1.DeviceJjApplication.documentation0=Documentation/STMicroelectronics.X-CUBE-MEMS1_GettingStarted.pdf
STMicroelectronics.X-CUBE-MEMS1.5.2.1.DeviceJjApplication.group0=Application
STMicroelectronics.X-CUBE-MEMS1.5.2.1.DeviceJjApplication.paramName0=ApplicationCcDeviceJjApplication
STMicroelectronics.X-CUBE-MEMS1.5.2.1.DeviceJjApplication.sevirity0=none
STMicroelectronics.X-CUBE-MEMS1.5.2.1.DeviceJjApplication.variant0=IKS01A2_DataLogTerminal
STMicroelectronics.X-CUBE-MEMS1.5.2.1.DeviceJjApplication_Checked=true
STMicroelectronics.X-CUBE-MEMS1.5.2.1.DeviceJjApplication_apiSize=1
STMicroelectronics.X-CUBE-MEMS1.5.2.1.DeviceJjApplication_bundle=Application
STMicroelectronics.X-CUBE-MEMS1.5.2.1.DeviceJjApplication_class=Device
STMicroelectronics.X-CUBE-MEMS1.5.2.1.DeviceJjApplication_name=X-CUBE-MEMS1
STMicroelectronics.X-CUBE-MEMS1.5.2.1.DeviceJjApplication_size=1
STMicroelectronics.X-CUBE-MEMS1.5.2.1.DeviceJjApplication_vendor=STMicroelectronics
STMicroelectronics.X-CUBE-MEMS1.5.2.1.DeviceJjApplication_version=5.2.1
STMicroelectronics.X-CUBE-MEMS1.5.2.1.IPParameters=MEMSCcBoardOoExtensionJjIKS01A2,ApplicationCcDeviceJjApplication
STMicroelectronics.X-CUBE-MEMS1.5.2.1.MEMSCcBoardOoExtensionJjIKS01A2=true
STMicroelectronics.X-CUBE-MEMS1.5.2.10.BSP.STBoard=false
STMicroelectronics.X-CUBE-MEMS1.5.2.10.BSP.api=BSP_BUS_DRIVER
STMicroelectronics.X-CUBE-MEMS1.5.2.10.BSP.component=
STMicroelectronics.X-CUBE-MEMS1.5.2.10.BSP.condition=SEMBoardOoExtensionJjIKS01A2
STMicroelectronics.X-CUBE-MEMS1.5.2.10.BSP.i2caddr=0
STMicroelectronics.X-CUBE-MEMS1.5.2.10.BSP.i2creg=
STMicroelectronics.X-CUBE-MEMS1.5.2.10.BSP.instance=I2C1
STMicroelectronics.X-CUBE-MEMS1.5.2.10.BSP.ip=I2C
STMicroelectronics.X-CUBE-MEMS1.5.2.10.BSP.mode=I2C
STMicroelectronics.X-CUBE-MEMS1.5.2.10.BSP.name=IKS01A2 BUS IO driver
STMicroelectronics.X-CUBE-MEMS1.5.2.10.BSP.semaphore=
STMicroelectronics.X-CUBE-MEMS1.5.2.10.BSP.solution=I2C1
STMicroelectronics.X-CUBE-MEMS1.5.2.11.BSP.STBoard=false
STMicroelectronics.X-CUBE-MEMS1.5.2.11.BSP.api=BSP_COMMON_DRIVER
STMicroelectronics.X-CUBE-MEMS1.5.2.11.BSP.component=
STMicroelectronics.X-CUBE-MEMS1.5.2.11.BSP.condition=
STMicroelectronics.X-CUBE-MEMS1.5.2.11.BSP.i2caddr=0
STMicroelectronics.X-CUBE-MEMS1.5.2.11.BSP.i2creg=
STMicroelectronics.X-CUBE-MEMS1.5.2.11.BSP.instance=PC13
STMicroelectronics.X-CUBE-MEMS1.5.2.11.BSP.ip=GPIO
STMicroelectronics.X-CUBE-MEMS1.5.2.11.BSP.mode=EXTI
STMicroelectronics.X-CUBE-MEMS1.5.2.11.BSP.name=BSP BUTTON
STMicroelectronics.X-CUBE-MEMS1.5.2.11.BSP.semaphore=
STMicroelectronics.X-CUBE-MEMS1.5.2.11.BSP.solution=PC13
STMicroelectronics.X-CUBE-MEMS1.5.2.12.BSP.STBoard=false
STMicroelectronics.X-CUBE-MEMS1.5.2.12.BSP.api=BSP_COMMON_DRIVER
STMicroelectronics.X-CUBE-MEMS1.5.2.12.BSP.component=
STMicroelectronics.X-CUBE-MEMS1.5.2.12.BSP.condition=
STMicroelectronics.X-CUBE-MEMS1.5.2.12.BSP.i2caddr=0
STMicroelectronics.X-CUBE-MEMS1.5.2.12.BSP.i2creg=
STMicroelectronics.X-CUBE-MEMS1.5.2.12.BSP.instance=USART2
STMicroelectronics.X-CUBE-MEMS1.5.2.12.BSP.ip=USART
STMicroelectronics.X-CUBE-MEMS1.5.2.12.BSP.mode=Asynchronous
STMicroelectronics.X-CUBE-MEMS1.5.2.12.BSP.name=BSP USART
STMicroelectronics.X-CUBE-MEMS1.5.2.12.BSP.semaphore=
STMicroelectronics.X-CUBE-MEMS1.5.2.12.BSP.solution=USART2
STMicroelectronics.X-CUBE-MEMS1.5.2.13.BSP.STBoard=false
STMicroelectronics.X-CUBE-MEMS1.5.2.13.BSP.api=BSP_COMMON_DRIVER
STMicroelectronics.X-CUBE-MEMS1.5.2.13.BSP.component=
STMicroelectronics.X-CUBE-MEMS1.5.2.13.BSP.condition=
STMicroelectronics.X-CUBE-MEMS1.5.2.13.BSP.i2caddr=0
STMicroelectronics.X-CUBE-MEMS1.5.2.13.BSP.i2creg=
STMicroelectronics.X-CUBE-MEMS1.5.2.13.BSP.instance=PA5
STMicroelectronics.X-CUBE-MEMS1.5.2.13.BSP.ip=GPIO
STMicroelectronics.X-CUBE-MEMS1.5.2.13.BSP.mode=Output
STMicroelectronics.X-CUBE-MEMS1.5.2.13.BSP.name=BSP LED
STMicroelectronics.X-CUBE-MEMS1.5.2.13.BSP.semaphore=
STMicroelectronics.X-CUBE-MEMS1.5.2.13.BSP.solution=PA5
STMicroelectronics.X-CUBE-MEMS1.5.2.1_BoardOoComponentJjMEMS_RteComponentsize=0
STMicroelectronics.X-CUBE-MEMS1.5.2.1_BoardOoExtensionJjMEMS_RteComponent0=\#define IKS01A2
STMicroelectronics.X-CUBE-MEMS1.5.2.1_BoardOoExtensionJjMEMS_RteComponentsize=1
STMicroelectronics.X-CUBE-MEMS1.5.2.1_BoardOoSupportJjSTM32CubeIiCustomIiBSPIiDrivers_RteComponentsize=0
STMicroelectronics.X-CUBE-MEMS1.5.2.1_DeviceJjApplication_RteComponent0=\#define IKS01A2_DATALOGTERMINAL_DEMO
STMicroelectronics.X-CUBE-MEMS1.5.2.1_DeviceJjApplication_RteComponentsize=1
STMicroelectronics.X-CUBE-MEMS1.5.2.1_MwName0=Application
STMicroelectronics.X-CUBE-MEMS1.5.2.1_NumberOfMw=1
STMicroelectronics.X-CUBE-MEMS1.5.2.1_SwParameter=ApplicationCcDeviceJjApplication\:IKS01A2IiDataLogTerminal;MEMSCcBoardOoExtensionJjIKS01A2\:true;
STMicroelectronics.X-CUBE-MEMS1.5.2.1_description=Drivers and sample applications for MEMS components
STMicroelectronics.X-CUBE-MEMS1.5.2.1_license=en.DM00367782.pdf
USART2.IPParameters=VirtualMode-Asynchronous
USART2.VirtualMode-Asynchronous=VM_ASYNC
VP_STMicroelectronics.X-CUBE-MEMS1_VS_BoardOoExtensionJjMEMS_5.2.1.Mode=BoardOoExtensionJjMEMS
VP_STMicroelectronics.X-CUBE-MEMS1_VS_BoardOoExtensionJjMEMS_5.2.1.Signal=STMicroelectronics.X-CUBE-MEMS1_VS_BoardOoExtensionJjMEMS_5.2.1
VP_STMicroelectronics.X-CUBE-MEMS1_VS_DeviceJjApplication_5.2.1.Mode=DeviceJjApplication
VP_STMicroelectronics.X-CUBE-MEMS1_VS_DeviceJjApplication_5.2.1.Signal=STMicroelectronics.X-CUBE-MEMS1_VS_DeviceJjApplication_5.2.1
VP_SYS_VS_Systick.Mode=SysTick
VP_SYS_VS_Systick.Signal=SYS_VS_Systick
board=NUCLEO-L053R8
boardIOC=true
2018-12-21 7:07 AM
Hi Mario,
you can try the IoC that I posted above (split in 2 pieces). It works fine on my side with CubeMX v5.0.0, MEMS pack v5.2.1 and CubeL0 v1.11.0. Obviously, in order to test it you need a Nucleo-L053R8 and a X-NUCLEO-IKS01A2.
Best Regards,
Carlo
2018-12-30 5:36 AM
I don't have X-NUCLEO-IKS01A2.
It seems that calling the function
MotionDrv[Instance]->GetCapabilities(MotionCompObj[Instance], Capabilities)
with parameters Instance = 0, Capabilities = NULL produces HardFault. - Because? - I'm not sure.
As much as I'm figured this out, There is no IKS01A2 connected so Capabilities stays NULL - it's updated to non of possible capability.
2019-01-07 2:34 AM
Hi Mario,
actually, if you try to debug the code, you should find that all the IKS01A2_***_Init functions fail when they check the WHOAMI id of the several MEMS components (if you do not plug the IKS01A2, you will obviously get an error for any I2C transaction). So, all the Init functions in your case will exit with an error code and they are not able to assign the driver APIs (like the GetCapabilities) to the instances of the MEMS sensors. This is the reason why you get an HardFault when you call the GetCapabilities. In the sample application the error management was neglected for simplicity, so the real program flow should stop after the first error in the IKS01A2_***_Init. Anyway, in my opinion, it does not make sense to test this code if you do not have the IKS01A2. I hope that this explains the behavior that you see.
Best Regards,
Carlo