cancel
Showing results for 
Search instead for 
Did you mean: 

Can you please tell me what IMUs have these top marks: SR010, SR919. I think they're in a 2.5mm x 3mm package.

DVarg.2
Associate

The top line has the SR. Then there's a 3D barcode, then the number 010 or 919.

1 ACCEPTED SOLUTION

Accepted Solutions
Eleon BORLINI
ST Employee

Hi @DVarg.2​ , you are right, the package dimension is that one. The device is a LSM6DSR. Please note that for ST IMU a standard marking codification is XXYZZ, where XX is the IMU part number, Y the last number of the LOT year and ZZ the year's week of the LOT. For example:

  • SR010 means LSM6DSR from week 10 '20 LOT.
  • SR919 means LSM6DSR from week 19 '19 LOT.
  • SO008 means LSM6DSO from week 08 '20 LOT.

-Eleon

View solution in original post

2 REPLIES 2
Eleon BORLINI
ST Employee

Hi @DVarg.2​ , you are right, the package dimension is that one. The device is a LSM6DSR. Please note that for ST IMU a standard marking codification is XXYZZ, where XX is the IMU part number, Y the last number of the LOT year and ZZ the year's week of the LOT. For example:

  • SR010 means LSM6DSR from week 10 '20 LOT.
  • SR919 means LSM6DSR from week 19 '19 LOT.
  • SO008 means LSM6DSO from week 08 '20 LOT.

-Eleon

DVarg.2
Associate

Thank you!!