2020-12-15 01:37 PM
Solved! Go to Solution.
2021-01-04 07:44 AM
Hello,
yes, it can be done. In attachment is simple example with LED function block. The input controls the LED2 (green LED) on SensorTile.box. If the input is equal to 1 the LED is on, otherwise is off. You can place the file to c:\Users\USER_NAME\STMicroelectronics\AlgoBuilder\Library\ directory, then is should be visible in AlgoBuilder application.
2021-01-04 07:44 AM
Hello,
yes, it can be done. In attachment is simple example with LED function block. The input controls the LED2 (green LED) on SensorTile.box. If the input is equal to 1 the LED is on, otherwise is off. You can place the file to c:\Users\USER_NAME\STMicroelectronics\AlgoBuilder\Library\ directory, then is should be visible in AlgoBuilder application.
2021-01-12 10:12 AM
Thank you again Miroslav!