cancel
Showing results for 
Search instead for 
Did you mean: 

Can I use STLINK-V3MINI with STEVAL-MKSBOX1V1

RChan.4
Associate
 
1 REPLY 1
Eleon BORLINI
ST Employee

Hi @RChan.4​ ,

I'm afraid that you can't -at least in a straightforward way-, since the SensorTile.box is 1.8V level compatible and the STLINK-V3MINI uses 3.3V.

You can however use the STLINK V3 adding a "level shifter" adapter to the main board: the part number of this device is B-STLINK-VOLT.

-Eleon