cancel
Showing results for 
Search instead for 
Did you mean: 

Solder mask opening for LGA 12 LIS2DE12 ?

antonius
Senior

Dear Members,

I want to create a solder mask for LIS2DE12,

Is my solder mask correct ?

Have a look on my screen shot, thanks

0693W000008wL2uQAE.png0693W000008wL2kQAE.png

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
Eleon BORLINI
ST Employee

Hi @antonius​ ,

it looks ok, check please your layout is compliant with the C and D rules (0.1m guard-band) of the TN0018 technical guidelines for the soldering that you reported.

The only issue you might face could be:

  1. If the solder paste quantity is small, the risk is that it could be not well dispensed under the inter-connected pads (not a huge risk, indeed);
  2. If the solder paste quantity is huge, you have to check that it doesn't flow out of the openings.

-Eleon

antonius
Senior

Do I need to add extra 0.1m ?

is solder mask at top solder (solder mask expansion ==>Specify expansion value? Add extra 0.1mm ?

0693W000008wSxiQAE.png

I can not see solder mask between pad, is that ok ? will it make a solder bridge? thanks

Eleon BORLINI
ST Employee

>> Do I need to add extra 0.1mm?

I think you should not, since the spacing between the pads (the black area in your previous picture) looks ok.

Of course, additional 0.1mm would prevent issues in case of an over-dispensing of of solder paste.

-Eleon