cancel
Showing results for 
Search instead for 
Did you mean: 

Can i use LSM6DSO MEMS with 6KHz odr with i2c bus?

DTali
Associate II

I see that i2c operate up to 400Hz

4 REPLIES 4
Ozone
Lead III

You might want to check if a read-multiple-bytes scenario provides enough bandwidth.

Just add up the number of transfer cycles required, and compare it to the time frame of a 6kHz update rate.

In SPI mode, the LSM6D allows up to 10MHz.

DTali
Associate II

With SPI everything is ok. Question is can i reach same ODR with i2c?

> Question is can i reach same ODR with i2c?

So check it by doing said calculation, or an appropriat software implementation.

Such bandwidth calculations are the SW engineering standard tasks.

it looks that everything is ok. i will also try fifo mode to increase productivity.