cancel
Showing results for 
Search instead for 
Did you mean: 

Can I cover Vl53l0X sensor with any type of cover for protection from environment?

Shubham Shivarkar
Associate II

Using this sensor in medical application due to which I can't install this sensor in open and therefore have to cover it with some material which will not harm its sensitivity and sensor will also be protected.

Thank you for helping.

1 ACCEPTED SOLUTION

Accepted Solutions
John E KVAM
ST Employee

Yes, you can. Glass, acrylic, PMMA and polycarbonate are good choices. Most plastics are transparent to 940nm light so this list is not exhaustive.

The trick is that even the best materials are not 100% transparent - and that leads to crosstalk.

Not to worry, though. Read the section on crosstalk correction and you can see how to compensate for it.


If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.

View solution in original post

1 REPLY 1
John E KVAM
ST Employee

Yes, you can. Glass, acrylic, PMMA and polycarbonate are good choices. Most plastics are transparent to 940nm light so this list is not exhaustive.

The trick is that even the best materials are not 100% transparent - and that leads to crosstalk.

Not to worry, though. Read the section on crosstalk correction and you can see how to compensate for it.


If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.