Skip to main content
Visitor II
August 14, 2024
Solved

Can be ASILB-LIBRARY used with single ASM330LHB sensor?

  • August 14, 2024
  • 1 reply
  • 766 views

Hello,

we're considering to use ASM330LHB in the SIL2 functional safety application and we would like to use and take credit from ST's ASILB-LIBRARY. However ASILB-LIBRARY use-case as it's documented expects that two redundant senors will be employed. Can be ASILB-LIBRARY used only with single IMU source? 

Thank you for the answer and support

@Denise SANFILIPPO thank you for your awesome article on this topic https://community.st.com/t5/mems-and-sensors/how-to-augment-your-automotive-safety-applications-with-the-imu/ta-p/670346 

This topic has been closed for replies.
Best answer by Federica Bossi

Hi @KSzurman ,

Welcome to ST Community!

The ST ASIL B solution is made up of an ASIL B software library called ASM330LHBxx_ASILB_library, certified by the third party TÜV, and two identical IMUs (either 2x ASM330LHB or 2x ASM330LHBG1).

The ASIL B software library implements software safety mechanisms which allows the overall solution, which is made up of hardware (two redundant IMUs) + software library, to be ASIL B compliant. 

So ASILB-LIBRARY cannot be used only with single IMU. 

1 reply

Federica Bossi
Federica BossiBest answer
ST Technical Moderator
August 14, 2024

Hi @KSzurman ,

Welcome to ST Community!

The ST ASIL B solution is made up of an ASIL B software library called ASM330LHBxx_ASILB_library, certified by the third party TÜV, and two identical IMUs (either 2x ASM330LHB or 2x ASM330LHBG1).

The ASIL B software library implements software safety mechanisms which allows the overall solution, which is made up of hardware (two redundant IMUs) + software library, to be ASIL B compliant. 

So ASILB-LIBRARY cannot be used only with single IMU. 

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.