2020-07-29 06:05 AM
I found this new application note online.
It is very interesting, and I wanna to implement it on my own STEVAL-BCN002V1B bought from digikey.
So can someone share the source code? Thanks.
2020-07-29 06:59 AM
Is it the right place for this question?
2020-08-17 07:10 PM
We have also found the PDF describing using BTLE for social distancing, it's the code that implements it that we're after as well.
My investigation has succeeded in generating beacons with the data I require using aci_gap_set_discoverable() but my use of aci_gap_start_general_discovery_proc() or aci_gap_start_limited_discovery_proc() to scan both return error 12 and the UM1865 document only describes that as "ERR_COMMAND_DISALLOWED" with no context to persue it further.
Does anyone have a bright light that will illuminate this issue?