2018-04-04 03:09 AM
Hi,
I have the sensortile
development kit
, I wanted to test the battery life without soldering the sensortile to the cradle board, without using USB charge and with the accelerometer always active. Does anyone who has used this sensor have an idea of how long it lasts battery?Thanks
Daniele
#battery #steval-stlkt01v1 #sensortile #sensortile-kit #accelerometer #battery-charging #battery-life #test2018-04-05 03:57 AM
Nobody will be able to give you exact answer.
The current consumption depends on many things (which IC are switched on, CPU clock, CPU sleep mode, firmware, ...)
2018-04-11 04:52 AM
Hi Miroslav,
I have not changed firmware, cpu clock or sleep mode from the default values. I have only activated on the board the acceleration sensor and a BLE connection with an Android device.
Thanks
Daniele