cancel
Showing results for 
Search instead for 
Did you mean: 

ASM330LHH imu sensor

semiconductor_user
Associate III

hello,

i have few basic Question regarding accelerometer sensor.

1. accelerometer data coming from imu sensor that is 2's compliment data, so should i receive this data in signed integer or unsigned integer? 

2. i want to know whatever raw data is coming from this sensor resgistors of accelerometer that is mg/LSB or only g ? if it is mg/LSB then how i can covert into g (refer ±2g)?

3. formula of convert g into (-180° to 0 to 180°) ?

please refer below attached  code or screenshorts

10 REPLIES 10

Hi @semiconductor_user ,

I'm glad you solved it. Can you make a new post explaining this question better?

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.