2014-03-12 04:22 PM
I am interested in the LPS25H MEMS barometer chip, but I am having a hard time figuring out the footprint of the HCLGA-10L package.
Here is what is called out in the datasheet: I cannot decipher from his what the dimensions of the pads should be. I believe that e1/2 might give me the width, but I cannot determine the length. Maybe that's what B is supposed to mean, but I don't see it. Also, I found that there is a but cannot find one for the LPS25H. I realize it's a very new part, but this would help -- it provides some guidance on how the pads should be laid out. Can someone more mechanically inclined parse this for me? Thanks. #hclga-10l2014-03-15 06:28 AM
For reference, here is the figure of merit from the LPS331AP, which is a comparable part (though with worse resolution).
T1 and T2 give the dimensions of the pads, and the rest can be inferred easily. I suppose I should just use the LPS331AP instead...2014-08-08 02:33 AM
Getting support for ST is much harder than getting blood out of a stone. They are at Rev 3 of this data sheet and still haven't dealt with this problem.
Freescale make a couple of nice parts which are similar in price.2014-10-01 10:10 PM
Hello,
Infact we are going to improve the quality of the drawing with more details; The pad dimension you are looking for are: 0.30mm x 0.45mm (+/- 0.05 mm tolerance) You can find the LPS25H AN just below the LPS331AP , at this address Thank you for your questions