2021-01-26 2:48 AM
Is it stored in the FIFO when the threshold of the INT1_THS register is exceeded?
Or is it stored regardless of the threshold of the INT1_THS register?
Solved! Go to Solution.
2021-01-27 9:11 AM
Hi @HIMAM.1 ,
if you intend the mechanical threshold of an external event, there is no trace of the interrupt in the FIFO (the INT1_THS is a configurable mechanical threshold).
If you intend the programmable watermark level event (i.e. when the desired FIFO filling level configurable in the FIFO_SRC_REG (2Fh) register is reached), it can be enabled to generate dedicated interrupts on the INT2 (I2_WTM bit of CTRL_REG3 (22h)), as described in the datasheet p.17.
I suggest you also to check the example available on Github for the i3g4250d_fifo_read.c.
-Eleon
2021-01-27 9:11 AM
Hi @HIMAM.1 ,
if you intend the mechanical threshold of an external event, there is no trace of the interrupt in the FIFO (the INT1_THS is a configurable mechanical threshold).
If you intend the programmable watermark level event (i.e. when the desired FIFO filling level configurable in the FIFO_SRC_REG (2Fh) register is reached), it can be enabled to generate dedicated interrupts on the INT2 (I2_WTM bit of CTRL_REG3 (22h)), as described in the datasheet p.17.
I suggest you also to check the example available on Github for the i3g4250d_fifo_read.c.
-Eleon
2021-01-27 10:21 PM
thank you for your answer.
I got a better understanding with your answer.
I will also check the example.