cancel
Showing results for 
Search instead for 
Did you mean: 

LPS25HBTR pressure reading decreasing over time

2067
Associate

I have bought a MKI-165V1 to test LPS25HBTR,but I find that the pressure value is decreasing for a long time ,from 1014.117 to 1002.970 in an hour.It is not stable,the next is my initial code,what is the reason for it

uint8_t data = 0x90;
HAL_I2C_Mem_Write(&hi2c4, 0xB8, 0x20 , I2C_MEMADD_SIZE_8BIT, &data, 1, HAL_MAX_DELAY);
HAL_Delay(10);
data = 0x00;
HAL_I2C_Mem_Write(&hi2c4, 0xB8, 0x21 , I2C_MEMADD_SIZE_8BIT, &data, 1, HAL_MAX_DELAY);
// HAL_Delay(10);
// HAL_I2C_Mem_Write(&hi2c4, 0xB8, 0x22 , I2C_MEMADD_SIZE_8BIT, pData, Size, 0xFF);
HAL_Delay(10);
HAL_I2C_Mem_Write(&hi2c4, 0xB8, 0x23 , I2C_MEMADD_SIZE_8BIT, &data, 1, HAL_MAX_DELAY);
HAL_Delay(10);
4 REPLIES 4
Federica Bossi
ST Employee

Hi @2067 ,

Can you please implement our official drivers and let me know if you still have the problem?

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

I think this sensor doesn't have many registers, so there's no need to use the official driver. Are there any other reasons for this, or are there any stable sensor configurations you would recommend?

Hi @2067 ,

It was just a way to check that your fw was correct.

Do you have a reference sensor with which you measure humidity?

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

I am measuring atmospheric pressure with the sensor, and I am currently taking measurements at an altitude of 120 meters indoors. However, without a reference firmware, I have noticed that the sensor readings can vary by more than 10 hPa in the same environment. I would like to know what might be causing this.