• Images in Public (Denise SANFILIPPO)

Images in Public (Denise SANFILIPPO)

  • Albums
  • All Images
Album Privacy: Public
  • « Previous
    • 1
    • …
    • 21
    • 22
    • 23
    • …
    • 41
  • Next »

Public (Denise SANFILIPPO)

  • Picture9.png
  • Figure 8: The .ucf file generated by MEMS-Studio can be imported in the High Speed Datalog GUI to test it with real time data
  • Figure 9: We can see the result at 0 when there is no movement: this is the stationary class
  • Figure 10: We can see the result at 4 when there is pick and place movement: this is the pick and place class
  • Figure 11: We can see the result at 8 when there is anomaly detection: this is the anomaly class
  • Figure 12: MEMS-Studio can be used also for evaluation with the compatible boards, for instance the Professional MEMS tool board
  • Figure 13: In the Quick Setup section of MEMS-Studio, ISM330BX can be easily configured and the evaluation mode can be changed to sensor fusion
  • Figure 14: In the 3D model section of MEMS-Studio, the sensor fusion low power running on ISM330BX can be evaluated
  • Figure 15: In FFT section of MEMS-Studio, the Fast Fourier transform of the data coming from the accelerometer and gyroscope of ISM330BX can be evaluated
  • Figure 16: Ecosystem of the IMU ISM330BX
  • Figure 4: In the MLC tool of MEMS-Studio, the three files generated can be imported with their label
  • Figure 1: The datalog we have previously acquired using High Speed Datalog is converted to a compatible format to be imported in MEMS-Studio
  • Figure 4: In the MLC tool of MEMS-Studio, the three files generated can be imported with their label
  • image (5).png
  • DeniseSANFILIPPO_2-1730390187048.png
  • DeniseSANFILIPPO_1-1730390187040.png
  • DeniseSANFILIPPO_0-1730390187038.png
  • DeniseSANFILIPPO_3-1730390187053.jpeg
  • DeniseSANFILIPPO_5-1730390187058.jpeg
  • DeniseSANFILIPPO_4-1730390187056.jpeg
  • Figure 1:  Data are collected using a LSM6DSO16IS smart IMU mounted with these orientations
  • Figure 1: Wand to hold SensorTile.box PRO, printed with 3D printer
  • Figure 2: SensorTile.box PRO
  • Figure 3: STEVAL-MKI229A (LSM6DSO16IS adapter board for a standard DIL24 socket)
  • Figure 4: ISPU magic wand
  • Figure 5: Gesture recognition for the the four letters I-S-P-U
  • Figure 6: ISPU magic wand model
  • Figure 6: ISPU magic wand model
  • DeniseSANFILIPPO_2-1730891152518.png
  • DeniseSANFILIPPO_0-1730891152487.png