cancel
Showing results for 
Search instead for 
Did you mean: 

X-CUBE-BLE2 Virtual_COM_Port does not work (X-NUCLEO-BNRG2A1)

a28j
Associate II

Hi, I am trying to use a X-NUCLEO-BNRG2A1 with a NUCLEO-L476RG .

I have used projects of X-CUBE-BLE2 with STM32Cube IDE. When I use sampleApp and SensorDemo_BLESensor-App it work, but Virtual_COM_Port doesn't.

The project successfully built and uploaded into the MCU, however no Com port appears and neither does bluetooth, it does not do anything.

Even if I copy directly the binary file into the "NUCLEO" device I see in Computer directly without using STM32Cube IDE, it doesn't work.

Any help would be appreciated.

1 REPLY 1
PChia.2237
Senior

Have you solved? i have same problem with nucleo re401