Question
aci_gatt_update_char_value for 20 bytes structs
I have an issue with an aci_gatt_update_char_value call to update a 20 byte characteristics.
So I defined a data struct that holds all my values.
typedef struct data {
uint16_t var1;
uint16_t var2;
uint16_t var3;
uint32_t var4;
uint16_t var5;
uint16_t var6;
uint16_t var7;
uint16_t var8;
uint16_t var9;
} dataset;and then call the update function (*data is a pointer to the initialized struct)
ret = aci_gatt_update_char_value(service_handle_runtime, char_handle_du, 0, 20, (uint8_t*)&data);If I define the struct only containing uint8_t or uint16_t everything arrives as expected. But with the uint32_t value I get somehow an offset or whatever.
Are there any restrictions when I have a characteristic with 20 bytes?