cancel
Showing results for 
Search instead for 
Did you mean: 

What is the status of the SPBTLE-RF BLE module ?

AndyJT
Associate III
Posted on June 27, 2018 at 16:46

Hi,

We're just completing a design based on the ST BlueTooth Low Energy module 

SPBTLE-RF.

However, we are finding it very difficult to find any stock (in the UK at least)

SPBTLE-RF is marked as not recommended for new designs

SPBTLE-RFTR looks ok and appears to be just a different format (Tape & Reel)

But delivery times are anything from 5 weeks to a year !

Nucleo development boards for BLE are still featuring this module so I presume it isn't going to be superseded anytime soon ? 

Thanks for any info anyone may have..

#ble #spbtle-rf
7 REPLIES 7
Posted on June 27, 2018 at 17:06

Packaging apart (tray vs T&R), modules are exactly the same.

XNucleo board will (can) mount TR modules if/when needed

Mark Bauman
Associate
Posted on June 28, 2018 at 02:12

I am seeing the same problem of availability here in the U.S. 

Any information on long term availability would be helpful.

AndyJT
Associate III
Posted on June 28, 2018 at 09:41

We can find the 

SPBTLE-RF0 much easier here, so will be testing that in the design.

As far as I can see, the only differences are in certifications and Tx/Rx current consumption unless anyone knows anything different ?

Thanks

Posted on June 28, 2018 at 11:48

RF/RFTR: SMPS power supply, LSE (32KHz) crystal, TELEC (Japan) certification

RF0/RF0TR: LDO power supply, no LSE crystal

Posted on June 28, 2018 at 12:29

Thanks for the info.

Does that mean the datasheet is wrong...

0690X0000060LWKQA2.png
Posted on June 28, 2018 at 13:22

Do not confuse BlueNRG's mandatory HSE (16, or 32MHz here) with optional LSE (32KHz)

Posted on June 28, 2018 at 13:43

Sorry, I immediately read it as 32Mhz, not Khz.

Thank you