cancel
Showing results for 
Search instead for 
Did you mean: 

Using X-NUCLEO-IDB04A1 with BlueNRG GUI fails

phorn9
Associate

Posted on November 11, 2016 at 15:16

Hi

I want to evaluate BlueNRG using the BlueNRG GUI. My setup is as follows:

  • NUCLEO-F401RE with X-NUCLEO-IDB04A1 installed.
  • BlueNRG GUI software version V2.2.1 (latest)
  • X-CUBE-BLE1 Cube Expansion package

I've followed the instructions found in the

http://www.st.com/content/ccc/resource/sales_and_marketing/presentation/product_presentation/19/93/09/fe/c2/90/49/09/X-NUCLEO-IDB04A1_quick_guide.pdf/files/X-NUCLEO-IDB04A1_quick_guide.pdf/jcr:content/translations/en.X-NUCLEO-IDB04A1_quick_guide.pdf

 and copied Virtual_COM_Port_F401RE.bin the the nucleo drive.

The virtual comm port appears and I can open it from BlueNRG GUI but BlueNRG GUI keeps asking:

''No Firmware detected on the motherboard. Update motherboard Firmware (under Tools menu).''

The proposed firmware installation procedure seems to be targeted at the STEVAL-IDB007V1 BlueNRG-1 development kit and fails with my setup.

Can anyone provide a hint how to get BlueNRG GUI working with the X-NUCLEO-IDB04A1?

Thanks!

11 REPLIES 11
phorn9
Associate
Posted on November 11, 2016 at 18:53

OK, found it. The problem occurs when an USB hub is between the PC and the Nucelo board. Everything works when the board is connected directly to the PC.

Dogan Yuksel
Associate
Posted on February 07, 2018 at 21:00

Ä° take same problem. I did not solve this.I am using same board and did same steps. I have just one different Bluetooth kit which is IDB05A1. How can you connect board directly 

Posted on February 08, 2018 at 11:28

Dear Dogan Yuksel,

what STM32 Nucleo board are you using with your X-NUCLEO-IDB05A1? And which version of ST-LINK/V2-1 do you have on your Nucleo?

In order to use the BlueNRG GUI, your STM32 Nucleo must be running the Virtual_COM_Port application.

If you have any issues when connecting to the BlueNRG GUI, I suggest to update the ST-LINK/V2-1 of your STM32 Nucleo. You can use either the STM32 ST-LINK Utility or the newer STM32CubeProgrammer for this.

Best regards,

Antonio

Girish Karnavat
Associate II
Posted on February 16, 2018 at 15:18

How to connect 

BlueNRG GUI to SensorTile Board?  Anyone did it?

Posted on February 16, 2018 at 16:37

Hello Girish Karnavat,

please find attached a binary image for the SensorTile that allows you to use theBlueNRG GUI.

You just need to program your SensorTile with it and then, from the BlueNRG GUI, you can open the VCOM port of your SensorTile.

Best regards,

Antonio

________________

Attachments :

SensorTile_BLE_Updater_VCP svn126.bin.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006Hxxv&d=%2Fa%2F0X0000000b2q%2FNIto6Vv18CneQGimtyGAbfGpD5Fry9IYULz6x_hpLKE&asPdf=false
Posted on February 16, 2018 at 18:06

Hi Antonio,

What flash address this binary should be flashed? 0x08000000 or  0x08004000?

Thanks,

Girish

Posted on February 16, 2018 at 18:21

You can flash it at 0x08000000 with either the STM32 ST-LINK Utility or the STM32CubeProgrammer.

If you don't have any of these tools already installed and are using an STM32 Nucleo to program it, as an alternative you can also drag-n-drop the bin file to the virtual mass storage disk of your Nucleo.

Best regards,

Antonio

Posted on February 16, 2018 at 20:04

Hi Antonio,

I un-installed BlueNRG GUI application, and downloaded new one and trying to install it as an Administrator, But observed that it is failing in installing the Virtual COM driver on Windows10 machine.

Do you have BlueNRG GUI forWindows 10? or PC Virtual COM driver for Windows 10?

Enclosed picture for your quick reference

Thanks,

Girish

________________

Attachments :

DriverInstallationFails.JPG : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006Hxxq&d=%2Fa%2F0X0000000b2p%2FjuBJf.QAiA.Ox0DJwoIuIW.fxHCgZAZdMMHXz6GOl2E&asPdf=false
Girish Karnavat
Associate II

Posted on February 20, 2018 at 21:48

Finally the BlueNRG GUI worked.

Need to install first

 

-2.6.0.0-Setup

on PC followed by

https://my.st.com/content/my_st_com/en/products/embedded-software/evaluation-tool-software/stsw-bluenrg-dk.html

, and test board programed with the above firmware

<LINK NO LONGER ACTIVE>

at

0x08000000 using STLink

than BlueNRG GUI v2.6.0 works.

Good Exercise...

Thanks

Girish