cancel
Showing results for 
Search instead for 
Did you mean: 

updated UM1755 doc?

philippe1
Associate II
Posted on February 03, 2015 at 08:49

Hi everyone, 

I was wondering if there is an updated version for the UM1755 which (partially) describes the commands available for the BlueNRG chipset. I can't find decoding scheme for the VS HCI events for example.

Thank you.
11 REPLIES 11
namoaton
Associate II
Posted on January 13, 2016 at 19:43

Could you please help me with this frame ?

Thank you.

04 ff 03 01 00 01

Posted on January 15, 2016 at 12:40

Dear Customer,

here below the description:

0x04- Event type

0xff - HCI_VENDOR;

0x3-Parameter Total Length;

0x01,0x00 - (0x0001 little endian) - Evt_Blue_Initialized

01 - Reason_Code ->Firmware started properly

This event occurs when the BlueNRG-MS firmware is started normally, it gives a Evt_Blue_Initialized event to

the user to indicate the system has started (with Reason Code 0x01).

Regards,

GM

Could you please help me with this frame ?

Thank you.

04 ff 03 01 00 01