cancel
Showing results for 
Search instead for 
Did you mean: 

STEVAL-IDP004V1 USB Function: Unable to determine what function does the usb port on the I/O Link board serves.

ASaee.1
Associate II
 
1 REPLY 1
Winfred LU
ST Employee

USB, RS-485, and CAN on the STEVAL-IDP004V1 are provided for more flexibility, which can be used for data exchange with additional units and with multiple sensor connections on the STEVAL-IDP003V1.

In the evaluation firmware, PC_Communication_USB project is to manage command decoding and data exchange between the STEVAL-IDP004V1 and a PC.