2019-07-08 12:31 AM
Dear all, I am new to STEVAL-BCN002V1.
I will like to inquire if there is any workshop presentation materials or materials which can explain to me the code walk-through for the entire STEVAL-BCN002V1.
As I will only use acclerometer and pressure sensor to get free-fall function, step counter, acitivites recongition.
Also, I will like to ask why am I able to add the customised C code which I had build using algobuilder to the whole project.
Please teach.
Best Regards
Gary
2019-07-10 10:36 PM
Hi Gary,
Please start from: STEVAL-BCN002V1B QUICK START GUIDE
https://www.st.com/resource/en/product_presentation/steval-bcn002v1b_quick_start_guide.pdf
Then, in after unpack the DK, there is a folder Docs with documents for your needs.
There are also user manuals or application notes available on ST web site:
https://www.st.com/en/wireless-transceivers-mcus-and-modules/bluenrg-1.html
Yes. You are able to customized firmware (C source code) for the projects.
Thank you.
Best Regards,
Winfred