cancel
Showing results for 
Search instead for 
Did you mean: 

ST87M01 startup sequence

Thierry Didi
Associate III

Hello

I am looking at the ST87M01 Startup sequence in ST87MXX Startup Application Note.

For configuring the ST87M01 (Band locks, eDRX, PSM ...), I understand that I need to "Stop the NBIOT Stack", enter my configuration with AT Commands, store this configuration in flash and restart the module.

  • is this correct ?
  • How do I "stop the NBIOT Stack" ?
  • Is it possible to bypass this automatic startup, i.e. send a first "AT command" at startup, execute a specific set of configuration commands, trigger the network attachment ... without rebooting ?

Many thanks,

Thierry

1 ACCEPTED SOLUTION

Accepted Solutions
Didier HERROUIN
ST Employee

Dear Thierry Didi,

It depends on the number of powers up you have in mind, as the number of flash writing cycles is limited as you mentioned it.

Nevertheless, after a Power Sleep Mode or a "clean" power off (triggered with AT#poweroff" command), the parameters will be saved inside the ST87M01 NVM, so you have no reason to re-load them.

If you think about the first power-up, a network breakdown, or an exceptional case requesting recovery like the modem can not attach anymore to the network , reloading your configuration and applying a AT#RESET=1 is a good solution.

Best regards, 


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

View solution in original post

6 REPLIES 6
Didier HERROUIN
ST Employee

Dear Thierry Didi,

The sequence is visible in the startup Application Note (slide 5).

You can stop the NBIOT stack by sending AT command : "AT+CFUN=0" (see on the right of the slide).

Then, if you modify the configuration, you must always send "AT#RESET=1" to save your parameters in the NVM (indeed, the reset is mandatory).

As reminder, for complete documentation, you must install the GUI (STSW-ST87MGUI :(at installation, it will create a folder containing numerous Application Notes). If you face difficulties to find this folder, you can access it via the "Help" menu in the GUI.

Best regards.


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Thierry Didi
Associate III

Hello Didier,

thanks for your reply - I have access to the documentation. I still have one question :

  • When my CPU starts, I want to be sure that the ST87M01 configuration is the configuration that I need. But since the ST87M01 starts with whatever config is stored in its flash, I cannot be sure that this is what I need. This is the reason why I was planning to reconfigure the ST87M01 each time my CPU restarts:
  • From your email, I see two solutions:
    • Reconfigure the ST87M01 each time my CPU starts, and reset the ST87M01 again with AT#RESET=1 if I understand your reply. It's a bit strange since this might lead to 2 ST87M01 resets at each startup, and also might cause to write in ST87M01 flash too often.
    • Send AT+CFUN=0, Read the actual config, and then AT+CFUN=1 if the config is the right one

Is one of these options the right one ? Or maybe there is another option ?

Many thanks

Thierry

Didier HERROUIN
ST Employee

Dear Thierry Didi,

It depends on the number of powers up you have in mind, as the number of flash writing cycles is limited as you mentioned it.

Nevertheless, after a Power Sleep Mode or a "clean" power off (triggered with AT#poweroff" command), the parameters will be saved inside the ST87M01 NVM, so you have no reason to re-load them.

If you think about the first power-up, a network breakdown, or an exceptional case requesting recovery like the modem can not attach anymore to the network , reloading your configuration and applying a AT#RESET=1 is a good solution.

Best regards, 


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Thierry Didi
Associate III

Thanks Didier,

I was thinking of any startup which might happen during the whole life of the product (several years), and where we are not sure of the previous modem state.

anyway, I think that your reply is quite clear. The modem starts with whatever params are in its NVM, and a AT#RESET=1 or AT#POWEROFF is required if we want to modify them.

Best Regards

Thierry

 

Just a short correction about your last comment : you should send "AT+CFUN=0" to stop the stack, modify the configuration according to your needs, and finally send "AT#RESET=1" to save the configuration and reboot the module.

AT#PWROFF is the command to power off the module with a clean network detachment, saving NVM parameters.


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Thierry Didi
Associate III

ok thanks for the clarification,

best regards

Thierry