2017-12-11 09:14 AM
hi,
is it possible to limit a connection to the module with one client?
wifi module is miniAP mode and HTTP server application run with web pages html.
One client connect to the wifi module
+WIND:28:Station Associated:44:85:00:F8:B6:DC:0
and i don't want a second client to connect in the same time of client1.
+WIND:28:Station Associated:08:11:96:9D:5E:D8:0
thks
Yoann
Solved! Go to Solution.
2017-12-11 09:33 AM
miniAP embedds a DHCP server. You can set the number of delivered IP addresses (ip_num_clients) to just 1. This way second STA can associate, but will be disassociated while client #1 is still in
2017-12-11 09:33 AM
miniAP embedds a DHCP server. You can set the number of delivered IP addresses (ip_num_clients) to just 1. This way second STA can associate, but will be disassociated while client #1 is still in