2016-07-05 12:41 AM
Hi
I have two SPWF01Sh device is installed between the communication method ofserverAT + S.SSIDTXT = SPWF_APAT + S.SCFG = wifi_priv_mode, 1AT + S.SCFG = wifi_wep_keys [0] 7465737431AT + S.SCFG = wifi_wep_key_lens, 05AT + S.SCFG = wifi_mode, 3AT & WAT + CFUN = 1AT + S.SOCKD = 32000, tclientAT + S.SSIDTXT = SPWF_APAT + S.SCFG = wifi_priv_mode, 1AT + S.SCFG = wifi_wpa_psk_text, test1AT + S.SCFG = wifi_mode, 1AT & WAT + CFUN = 1When wifi_priv_mode, 0 no problems if I set the type of protectionwifi_priv_mode, 1 �?lien can not connect network search+ WIND: 21: WiFi Scanning+ WIND: 35: WiFi Scan Complete (0x0)+ WIND: 21: WiFi Scanning+ WIND: 35: WiFi Scan Complete (0x0)during calibration using the command AT + S.SCAN BSS CC: 5D: 4E: 4D: EE: 4A CHAN: 11 RSSI: -87 SSID: 'SPWF_AP' CAPS: 0431ustanovlinoy no WEP protection is due to petsifikatsiey miniAP or am I not right tune?2016-07-05 04:45 AM
Both miniAP and STA need the same ''wifi_wep_key*'' settings
2016-07-05 05:15 AM
thank you helped this setting should have been on the client and server set
AT + S.SCFG = wifi_wep_keys [0] 7465737431AT + S.SCFG = wifi_wep_key_lens, 05