Skip to main content
sauli
Associate
Jul 1, 2016 9:38 AM UTC
Question

Not getting socket data pending indication (+WIND:55)

Posted on July 01, 2016 at 11:38

Working with the SPWF01SA.11 module.  In an attempt to make my program event based, I was trying to utilize the indications for reading data received from a socket.  But I am not getting the +WIND:55 indication although data is received:

1. Open a socket to a MQTT server (test.mosquitto.org) -> OK

2. Send a MQTT CONNECT packet -> OK

3. Wait for +WIND:55:Pending Data

10 seconds goes by with nothing at all received from the WiFi module

4. Close the socket -> ERROR: Pending data

5. Query pending data -> DATALEN: 4

6. Read four bytes -> Get exactly the response I was waiting for.

Same as a communication log:

AT+S.SOCKON=test.mosquitto.org,1883,t

 ID: 00

OK

AT+S.SOCKW=01,36

Send 36 bytes of socket data.

OK

AT+S.SOCKC=00

ERROR: Pending data

AT+S.SOCKQ=00

 DATALEN: 4

OK

AT+S.SOCKR=00,4

Read 4 bytes of socket data

OK

Why am I not getting the indication?  None of the indications is disabled.

The version date of the module was 150410, and since the ST website has a newer version 160129, I decided to update. The batch file in the update packet - after inputting the .bin file path and the serial port number - takes about an eyeblink to run to 'Press a key to exit...'. It gives no error messages, but obviously does not update the firmware either.

It does print a web address which lead me to Sourceforge stm32flash page.  I downloaded that program and ran it instead of 1203flash.exe used by the batch file. I used exactly the same command line arguments, and this time the binary file was programmed to the module.  Only, now the module is dead. How do I recover it?

The new version would be useful also because it supports error numbering in the ERROR response. Parsing the error code form the description string is unnecessarily tedious.

    This topic has been closed for replies.

    3 replies

    Gerardo GALLUCCI
    ST Employee
    Jul 4, 2016 9:14 AM UTC
    Posted on July 04, 2016 at 11:14

    If you need the indication, turn the indication on.

    AT+S.SOCKON=test.mosquitto.org,1883,t,ind

    About the stm32flash, I think you deleted the bootloader. Module is lost. Contact your direct support/distributor to get a recover image...

    sauli
    sauliAuthor
    Associate
    Jul 4, 2016 11:41 AM UTC
    Posted on July 04, 2016 at 13:41

    Ahh, I somehow managed to miss that ind. I didn't realize that you can control it by socket.

    About the recovery image.. Should I program it with stm32flash? And why didn't 1203flash work?  Do I ever again dare to try update the module firmware?

    Gerardo GALLUCCI
    ST Employee
    Jul 5, 2016 11:43 AM UTC
    Posted on July 05, 2016 at 13:43

    You can use stm32flash (the one given by ST, not the standard one from Google code) or STM32 Flash Loader Demonstrator. Contact ST to recover dead module