cancel
Showing results for 
Search instead for 
Did you mean: 

SPWF01S firmware update fail

k_ovchinnikov
Associate II
Posted on November 07, 2014 at 16:24

Hi. I'm using SPWF01S modules and I have trouble with it. The connection to router takes a big time amount. It's may take average 5, 10 or 30 minutes some time. So I dicided to update firmware.

For update I used Flash  Loader Demonstrator. But during firmare update I set 0x8000000 as a start address and my module is dead. Next update I performed with 0x8008200 as start adress, but module still not working.

Can I return it to alive state and how?

Thanks.
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Posted on November 18, 2014 at 11:20

Hi,

performing an update to 0x08000000 address, I think you deleted boot application of the module. Your module is dead.

I ask you to contact your local ST support. You need a full binary file.