cancel
Showing results for 
Search instead for 
Did you mean: 

SPSGRF-915 Different Marking questions

TLi.8
Associate II

Hi 

We got some parts of SPSGRF-915, they have different Marking 1 and Marking 2, I attached photos for your reference.

Marking 1: SPSGRF-915 (Full Marking and the label shows the Full MPN SPSGRF-915)

Marking 1.JPG

 

 

 


Marking 2: SPSGRF (Without “-915”, but the label shows the Full MPN SPSGRF-915)

Marking 2.jpg

 

What is the different?
We want to verify that Marking 1 and Marking 2 have the same functionality? 
Also, what mean for this different markings? Are they the same part?

Thank you

6 REPLIES 6
RhSilicon
Lead

Apparently the "-915" characters were made with a CNC drill. Perhaps both are clones. The datasheet shows the complete code made directly on the board layout:

SPSGRF.png

It is possible that different date codes produce different Marking?
We are concerned that they are not the same parts, can you provide some more accurate indication that they are clones.

Marking 1 Date Code is 23+
Marking 2 Date Code is 19+/18+

Where else can we verify that the MPN of Marking 2 must be SPSGRF-915?
We have to confirm that it is 915 MHZ frequency for sure.

RhSilicon
Lead

I found the status of Obsolete, maybe that's why some manufacturer could be reproducing it:

ST_NRND.png

Thanks for sharing this information. Yes, we know it's OBS part.
Anyway, do you know how to get engineer from STM to reply to this question?
We hope to get some more accurate PDF to verify it, or if STM engineers can approve it, then we will be more confident to use these parts.