2015-10-28 10:06 PM
Hi
In regards to using the SPIRIT1 device in the SMPS OFF mode (without internal switch-mode converter), it's not clear whether the 1.4-1.8V net connected to the SMPS Ext 2 pin is provided internally via an internal LDO, or is it mandatory to be supplied by an external 1.4-1.8V supply? Please advise which method should be taken. Thank you. Regards Heard. #spirit12015-10-29 4:55 AM
Hello,
It is mandatory supply 1.4-1.8V to the SMPS Ext 2 pin.Best Regards,S2015-10-29 6:47 AM
Thanks!