Posted on August 24, 2015 at 10:44Hello,Yes, it is not possible to know the exactly value of the RSSI while the radio is in RX state.So, the SPIRIT1 performs a loop like this: RX for about 2 sec, READY state due to SABORT command and then RSSI_LEVEL...
Posted on June 30, 2015 at 10:32Hello,Once the board is ON, You must be able to see the clock signal by probing directly the two pins of the crystal. If it is not, this means the crystal is not soldered correctly.Best Regards,S
Posted on June 29, 2015 at 11:07Hello,In all the pictures, the signals are clock and MISO. According to datasheet the value 0x06 means READY state and XO NOT OPERATING.Just try this test: - register 0x05, value 0x8A - register 0x06, value 0x80and ch...
Posted on June 29, 2015 at 08:03Hello,What does it mean the chip cannot switch to any other state, but ready?Have You tried sending a STANDBY command to put the SPIRIT1 in STANDBY state?At which command the SPIRIT1 does not respond? And what is the ...