cancel
Showing results for 
Search instead for 
Did you mean: 

Spirit1 How to Configure Intterupts

hacer
Associate II
Posted on March 16, 2015 at 08:21

Hi,

I use Spirit1 on my custom board that includes stm32l162 MCU. I am trying to work the ''BasicPktTest'' example. Actually I can view the packets are being transmitted and received between two devices. But it does not start the interrupts even though they are enabled in the example. I also checked the interrupt pin with an oscilloscope. It doesn't rise or fall while I run the project. Where can I get the information about configuration of interrupts in Spirit1?

Kind regards

#spirit1
1 REPLY 1
Nickname4815_O
Associate II
Posted on April 03, 2015 at 10:23

Please see discussion: Spirit1 IRQ Config