2015-03-16 12:21 AM
Hi,
I use Spirit1 on my custom board that includes stm32l162 MCU. I am trying to work the ''BasicPktTest'' example. Actually I can view the packets are being transmitted and received between two devices. But it does not start the interrupts even though they are enabled in the example. I also checked the interrupt pin with an oscilloscope. It doesn't rise or fall while I run the project. Where can I get the information about configuration of interrupts in Spirit1?Kind regards #spirit12015-04-03 01:23 AM
Please see discussion: Spirit1 IRQ Config