2022-03-14 01:19 PM
Hello Everyone,
I have my own board. I’m using Keil uVision5 and STSW-BNRGLP-DK DK-1.1.0 software package.
I have an issue when I try to migrate my own application from BlueNRG-355MC to BlueNRG-345MC. I have followed the steps in the User Manual:
Keil toolchain:
– in [Projects]>[Options for Target '...']>[Device]>[ST BlueNRG-LP Series]>[ST BlueNRG-LP], select
ST BlueNRG-345
– in [Projects]>[Options for Target '...']>[C/C++]>[Preprocessor Symbols]>[Define], add
CONFIG_DEVICE_BLUENRG_345
– in [Projects]>[Options for Target '...']>[Linker]>[Misc Control], add –predefine="-
DCONFIG_DEVICE_BLUENRG_345=1"
I am able to program a simple blinking led correctly, but my issue is when I want to use OTA configuration.
For my application I need to program first the firmware BLE_OTA_ResetManager and then program my firmware with Lower or Higher configuration. This works for me in BlueNRG-355.
I tried to migrate firmware BLE_OTA_ResetManager and my firmware following the steps, but I don’t get any result. Keil programs it correctly but the microcontroller does nothing.
Has anyone had the same issue?
Am I doing something wrong, or should it work migrating both apps, Reset_Manager and my own app?
I would appreciate any possible help
Thanks.
2022-04-20 10:29 PM
Hi ARami, I am facing a similar issue. Did you find any solution to make it work? Thanks!