2019-06-03 06:05 PM
2019-06-03 06:54 PM
I should first read the S2-LP data sheet completely before I was asking the question as I find the answer on it: " The Direct Polar Mode is suitable to implement differential binary phase shift keying modulation (DBPSK) such as the data modulation used by the SigFox protocol".
So this is a theoretical answer to how it is achieved !
Now it would be nice if there is
an example of register
configuration for such DBPSK (and encoded bytes which need to be sent to
TX_FIFO).
Can anyone help with this?