cancel
Showing results for 
Search instead for 
Did you mean: 

S2-LP: Correct procedure to change frequency?

Pieter Conradie
Associate III

Hi there!

What is the correct procedure to change the S2-LP's frequency after it has been initialized with a call to S2LP_RADIO_Init()?

After I call S2LP_RADIO_SetFrequencyBase() the S2-LP appears to lock up. MC_STATE1 = 0x52 and MC_STATE0 = 0x29 which means that the state value is an invalid value of 0x14 which indicates an error condition or hardware issue.

Thanks in advance,

Pieter

https://piconomix.com

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Pieter Conradie
Associate III

Apologies!! This is a bit embarrassing but the problem was between keyboard and chair :(

I tried to set the frequency to 869,000 Hz instead of 869,000,000 Hz. It's working perfectly now.

Regards,

Pieter

View solution in original post

1 REPLY 1
Pieter Conradie
Associate III

Apologies!! This is a bit embarrassing but the problem was between keyboard and chair :(

I tried to set the frequency to 869,000 Hz instead of 869,000,000 Hz. It's working perfectly now.

Regards,

Pieter