2014-10-15 2:36 PM
Is it possible / practical to reprogram a Spirit1 USB Dongle (STEVAL-IDS001V5) to operate within the band 921-929MHz (which is available for general use at 1W in New Zealand)?
If so what would be the approach, hardware/software needed? Views on this would be appreciated. Best wishes, Ron.2014-10-16 12:32 AM
Hello,
yes, it is possible to operate in the 921-929MHz band with the STEVAL-IDS001V5. Are you planning to use the GUI or to develop a custom firmware?and code examples
for SPIRIT1 firmware development. In order to use or modify the provided example projects, it is required to have installed IAR Embedded Workbench for ARM (v6.40 or above) and a JTAG interface like ST-LINKv2 or IAR JLink.2014-10-16 11:30 PM
Hi Gaetano
Very much appreciate your response. From what you say we should be able to use the device. We typically use open source tool chains rather than IAR, for example to programme STM32W108 USB dongles. Is there any reason why we should not do the same with the STEVAL-IDS001V5? Very best regards, Ron2014-10-17 12:27 AM
Hello Ron,
we use IAR, but you can use your favourite toolchain, clearly modifying it as needed.Best regards,Gaetano